Skip to main content
NITIN RAWAL
Associate
May 14, 2018 12:20 PM UTC
Question

TCP CLIENT USING NETCONN API SOMETIMES CONNECT.

Posted on May 14, 2018 at 14:20

Hello Every One,

I am writing a TCP client on STM32F427 MCU using netconn API. My device is able to connect three times out of ten times. it seems the problem with netconn_connect() api. please help with this.

Note:  

netconn_connect() is not coming back with any return value most of the times. 

void StartDefaultTask(void const * argument)

{

/* init code for LWIP */

MX_LWIP_Init();

IP4_ADDR(&local_ip,192,168,100,60);

IP4_ADDR(&remote_ip,192,168,100,61); //192.168.100.61

printf('\r\nremote ip adress:%s\r\n',ip4addr_ntoa(&remote_ip));

printf('\r\nlocal ip adress:%s\r\n',ip4addr_ntoa(&local_ip));

//netif_set_up(&gnetif);

conn = netconn_new(NETCONN_TCP);

printf('\r\n%d',conn);

printf('\r\nstate: %d',conn->state);// this is printing zeros every times

if((netconn_bind(conn,&local_ip,23))==ERR_OK)// bind to local device IP

{

printf('\nnetconn_bind succeed\n');

//vTaskDelay(100);

osDelay(10);

if((netconn_connect(conn,&remote_ip,23))==ERR_OK)// Connect to remoter FTP Server

{

printf('\nconnect\n');

osDelay(10);

netconn_write(conn, (char *)'12345678', 8, NETCONN_NOFLAG);

printf('\r\nstate: %d',conn->state);

osDelay(100);

netconn_write(conn, (char *)'12345678', 8, NETCONN_NOFLAG);

printf('\r\nstate: %d',conn->state);

osDelay(100);

netconn_write(conn, (char *)'12345678', 8, NETCONN_NOFLAG);

printf('\r\nstate: %d',conn->state);

osDelay(100);

netconn_close(conn);

netconn_delete(conn);

for(;;)

{

printf('\r\nHello');

osDelay(1000);

}

/* USER CODE END StartDefaultTask */

}
    This topic has been closed for replies.