Skip to main content
charles2399
Associate III
November 16, 2008
Question

SysTick Interrupt

  • November 16, 2008
  • 4 replies
  • 670 views
Posted on November 16, 2008 at 08:29

SysTick Interrupt

    This topic has been closed for replies.

    4 replies

    charles2399
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:50

    I am trying to use the systick example from the FW library.

    We are using the Green Hills suite and ST does not provide support for this tool set. So I have had modify the examplet for the Green Hills SW.

    Boot pins are 00, the vectors located at 0x2000e800 is SRAM.

    Still no interrupts.

    Any suggestion?

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:50

    Hi Charles,

    You get be inspired by using the

    http://www.st.com/stonline/products/support/micro/files/um0427.zip

    on web and then to this example : STM32F10xFWLib_v2.0.3\FWLib\examples\SysTick

    Cheers,

    STOne-32.

    charles2399
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:50

    I am having a problem getting the systick interrupt. Yes I new to ARM prducts.

    The SysTic control register shows the interrupt is enabled, count flag is 1, and mult-shot is enabled.

    The Interrupt Control State register shows systick interrupt is pending and the vector is 15.

    The I and F flags in CPS register are 0 (interrupts are enabled).

    Execution is out of sram and the vector tables is moved to 0x2000E800 and the TVOR register shows the correct vector table address.

    Does anyone know what is wrong?

    - Chuck

    stefan239955_stm1_stmicro
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:51

    In case you're using the stm32f10x_it.c/.h files from the example to handle the interrupt, there's a typo which you should fix:

    Code:

    void SysTickHandler(void)

    should be

    Code:

    void SysTick_Handler(void)