Question
Systick doesn't fires up as expected
Posted on November 15, 2011 at 14:39
I programmed the systick timer in order to get 1ms delay but I seem to get a 10us delay instead.
From the reference manual RM0008''The SysTick calibration value is set to 9000, which gives a reference time base of 1 ms with the SysTick clock set to 9 MHz (max HCLK/8).''I configured the system clock at 72Mhz and the AHB prescaler at 1. The clock source of the systick is also set to 1, thus clock core. Although I don't understand what it means by ''external reference clock''. I loaded up 9000 into the systick reload value.I wrote this simple routine to get a delaystatic uint32_t gCounter = 0;void sys_tick_timer(){ if (gCounter) gCounter--;}static void delayms(uint32_t millisecond){ gCounter = millisecond; while (gCounter > 0);}but the interrupt seems to be fired much faster then 1ms. I have to load 100*1000 valueto get a delay of about 1 second.Any suggestions would be appreciated.S.