Skip to main content
nickabrham
Associate II
April 19, 2012
Question

Systick Calibration

  • April 19, 2012
  • 5 replies
  • 1285 views
Posted on April 19, 2012 at 14:29

Hi,

I want to generate 10ms systick. According to the example code provide with the StdPeriph_Lib_V3.5.0 i.e. \Project\STM32F10x_StdPeriph_Examples\SysTick\TimeBase, the systick of 1ms can be easily generated by the following code

if (SysTick_Config(SystemCoreClock / 1000))

  {

    /* Capture error */

    while (1);

  }

I am running my STM3210E-EVAL at 72MHz. I was wondering how the following SysTick_Config(SystemCoreClock / 1000) could generate 1ms systick interrupt when the clock frequency is 72MHz. Kindly also tell me what divisor should I use in SysTick_Config function to generate 10ms interrupt.

bye,

Nick
    This topic has been closed for replies.

    5 replies

    frankmeyer9
    Associate III
    April 19, 2012
    Posted on April 19, 2012 at 15:41

    I suggest to debug into the SysTick_Config() function, and/or read the reference manual.

    SystemCoreClock is the frequency the core is clocked with - 72MHz in your case.

    (

    SystemCoreClock/1000

    ) means, you get a SysTick interrupt after 72.000.000 / 1000 timer counts. This way, the divisor gives you the number of SysTick interrupts per second.

    For 10ms, which means 100 ticks / sec., you need (

    SystemCoreClock/100

    ).

    Tesla DeLorean
    Guru
    April 19, 2012
    Posted on April 19, 2012 at 15:47

    A millisecond is 1/1000 th of a second, 10 ms is 1/100 th.

    SysTick_Config(SystemCoreClock / 100)

    Remember the SysTick clock is ticking in 1/72000000 th of a second units, unless you have it in HCLK/8 mode. You're counting the number of ticks that 10 ms would take.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    April 19, 2012
    Posted on April 19, 2012 at 15:48

    Beat me to the post there.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    amin23
    Visitor II
    April 19, 2012
    Posted on April 19, 2012 at 15:57

    Hi,

    To generate 10ms interrupt set the SysTick Reload Value register to (SystemCoreClock/100) that is mean SysTick_Config(SystemCoreClock / 100). here below an example:

    e.g: SystemCoreClock = xxMHz

    -  SysTick interrupt period = the Reload Value register divided by clock frequency

                                   = (SystemCoreClock/1000)/SystemCoreClock = 1/1000 = 1ms

    nickabrham
    Associate II
    April 20, 2012
    Posted on April 20, 2012 at 06:31

    Hi Everyone

    ,

    Thanks to all of you for explaining and giving solution to my query.

    Regards,

    Nick