Skip to main content
sylvain tremblay
Visitor II
April 3, 2018
Question

SystemClock_Config with Standart library for stm32f7xx

Posted on April 03, 2018 at 23:17

hello everybody,

I want to program a clock at 210 Mhz on a stm32f7xx. My parameters are:

HSI RC (16 Mhz) used 

PLL Source Mux , PLLM = /8, PLLN = * 210 , PLL /P = /2 , PLL /Q = 9 ( used for SD)

System Clock Mux PLLCLK ,  AHB = 1  So HCLK = 210 Mhz  

Also APB1 prescaler = 4 and 

APB2 prescaler = 4.

I use the standard library for stm32f7xx take on GITLAB do by decha.

The library is good, but i have a  problem. I can not choice the input System Clock Mux PLLCLK on the system clock mux.

I checked in the register, and the bits is good (RCC clock configuration register (RCC_CFGR)) but it not running.

the code is 

RCC_PLLCmd(DISABLE);

RCC_PLLI2SCmd(DISABLE);

RCC_PLLConfig(RCC_PLLSource_HSI, 8, 210, 2, 9);

RCC_HCLKConfig(RCC_SYSCLK_Div1);

RCC_PCLK1Config(RCC_HCLK_Div4);

RCC_PCLK2Config(RCC_HCLK_Div2);

RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);

RCC_PLLCmd(ENABLE);

RCC_PLLI2SCmd(ENABLE);

RCC_RTCCLKCmd(ENABLE);

while (RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET){};

while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET){};

RCC_GetClocksFreq(&PeriphClk);

SrcClk1 = RCC_GetSYSCLKSource();

RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);  the bit in the register is good, but the src is not good, the clk is not running goog???

Can you help me,

thank

S.T

    This topic has been closed for replies.