Skip to main content
L C
Associate III
September 19, 2018
Question

"System Workbench�?(SW4STM32) printf redirection not work

  • September 19, 2018
  • 1 reply
  • 888 views

Dear All

I would like to redirect printf output to UART.

It seem very simple in this field and many example in internet.

I try that with "System Workbench"(SW4STM32).

The IDE doesn't show anything wrong.

adding below to "uart.c" 

#ifdef __GNUC__
 /* With GCC/RAISONANCE, small printf (option LD Linker->Libraries->Small printf
 set to 'Yes') calls __io_putchar() */
 #define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#else
 #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)
#endif /* __GNUC__ */
/**
 * @brief Retargets the C library printf function to the USART.
 * @param None
 * @retval None
 */
PUTCHAR_PROTOTYPE
{
 /* Place your implementation of fputc here */
 /* e.g. write a character to the EVAL_COM1 and Loop until the end of transmission */
 HAL_UART_Transmit(&huart1, (uint8_t *)&ch, 1, 0xFFFF);
 
 return ch;
}

calling printf() in "main.c"

printf("\n\r UART Printf Example: retarget the C library printf function to the UART\n\r");

The "printf()" seem don't work in my chip.

But "HAL_UART_Transmit" is function in main.c. That imply the UART port work fine.

Then try adding something GPIO action(output toggle) inside the "PUTCHAR_PROTOTYPE" routine. If printf() running, "PUTCHAR_PROTOTYPE"(fputc() or __io_putchar()) should be call. The GPIO action hasn't execute, mean "PUTCHAR_PROTOTYPE" hasn't be call.

Is there any where necessary to modify for such redirection except "uart.c"?

My code is generated by STM32CubeMX and hasn't "syscall.c"

Is it a root cause of my problem?

Or System Workbench is not support printf() redirection?

Please share your comment.

BR

    This topic has been closed for replies.

    1 reply

    David SIORPAES
    ST Employee
    September 20, 2018

    Hello @L C​ ,

    you are right you'd need to add syscall.c (example attached) or directly implement

    int _write(int file, char *ptr, int len);