Skip to main content
lspr35
Associate II
March 19, 2009
Question

System Memory Boot Mode and TIM1 usage

  • March 19, 2009
  • 13 replies
  • 2138 views
Posted on March 19, 2009 at 07:35

System Memory Boot Mode and TIM1 usage

    This topic has been closed for replies.

    13 replies

    lanchon
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:18

    no and no.

    but you can make your own bootloader and keep it protected in a section of flash. too bad ST won't release the source of their bootloader, it'd make things easier for you. they do provide DFU code to flash via USB (but if your code must be secure, I wouldn't use it; it might have security issues in the form of exploitable bugs).

    j2_it
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:18

    Quote:

    1. it is possible to jump into the boot loader from your application. So you do not need to modify the BOOT0/BOOT1 pins.

    Wolfgang Beck

    It's possible with a jump to 0x1FFF F000?

    Are there configurations before jump?

    jerome

    [ This message was edited by: j.vaquie on 19-03-2009 12:05 ]

    wolfgang
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:18

    Hi,

    You are right. We finally failed to use the remapped USART1 for the boot loader.

    Has anyone there implent his own boot loader?

    Regards

    Wolfgang Beck