Skip to main content
bob239955
Associate III
Jan 15, 2009 1:22 PM UTC
Question

System Bootloader not working but UART1 works OK.

Posted on January 15, 2009 at 14:22

System Bootloader not working but UART1 works OK.

    This topic has been closed for replies.

    13 replies

    adrian3
    Associate II
    May 17, 2011 10:19 AM UTC
    Posted on May 17, 2011 at 12:19

    I'm just wondering - should Boot 1 be connected directly to ground as it doubles as Port B-2? What happens if you remove the pull up resistor R48, and connect to ground via a suitable resistor?

    matt1
    Visitor II
    May 17, 2011 10:19 AM UTC
    Posted on May 17, 2011 at 12:19

    Hi all,

    I seem to be having a similar problems to those described here.

    My RS232 transceiver was outputting garbage on the RS232 side until I added a pull-down to the TTL side. This seems to have resolved the problems with the bootloader.

    Is the Tx pin from the STM floating when in system bootloader mode until data is received on the Rx pin? This would seem strange.. but I can't see any other reason why the changes I made resolved the problem.

    Matt

    bsy006
    Associate II
    May 17, 2011 10:19 AM UTC
    Posted on May 17, 2011 at 12:19

    Hello, I see the Flash Loader Demonstrator 1.2 (not 1.0) works OK @ 115.2k

    STM' BootLoader is v2.0.

    Yuri.