Skip to main content
jeff moore
Associate
December 21, 2017
Question

synchronous non-multiplexed PSRAM

  • December 21, 2017
  • 3 replies
  • 1152 views
Posted on December 21, 2017 at 13:34

We are using STM32 microcontrollers that have a parallel data bus driven by on-board memory controller called FMC. This data bus has multiple operating modes and the one in which we are interested is synchronous non-multiplexed PSRAM. It must be synchronous, the RAM will have a clock input.

Focusing on the L4 and F7 series(only certain members of a product range have the FMC capability that depends on the package size).

To demonstrate that the bus is working properly, we would like to connect a synchronous RAM to the bus operating at 3.3V with a data bus width of 16 bits. The RAM needs to be mounted in such a way that it is easy to connect it to a target microcontroller with flying leads. I have had a good look and finding/sourcing a suitable RAM is proving very difficult as all PSRAM seems to be Asynchronous, some Cellular RAM and dual port RAM(would only need one port) does offer synchronous capabilities. Any help gratefully received

Thanks

J

    This topic has been closed for replies.

    3 replies

    waclawek.jan
    Super User
    December 23, 2017
    Posted on December 23, 2017 at 10:59

    it must be synchronous, the RAM will have a clock input.

    finding/sourcing a suitable RAM is proving very difficult as all PSRAM seems to be Asynchronous

    This is contradicting: do you have a RAM to interface to, or not? Why do you insist on synchronous memory?

    JW

    jeff moore
    Associate
    January 8, 2018
    Posted on January 08, 2018 at 10:59

    Hi we are interested in the operating mode

    synchronous non-multiplexed PSRAM operating modes, and no we don't have any RAM to interface to that is the question we are finding it very difficult to source any.

    thanks

    J

    waclawek.jan
    Super User
    January 8, 2018
    Posted on January 08, 2018 at 12:04

    If you just want some proof of concept device, you are then surely not interested in the particular capacity, are you? Then why don't you simply use an old-fashioned flow-through synchronous SRAM?

    JW