Sync problems between H7 cores
hello!
i am working with the stm32h745 dual core nucleo dev board.
currently, i am trying to create a constant pulse on a GPIO output pin which belongs to the M4 core every 40 ms.
when i run with the m4 alone the pulse is very accurate and looks perfect.
when i run both cores (m7, and m4) the pulse looses sync and dosent appear to be correct.
i do not understand this since i configured that gpio to belong to strickly m4, it is indipendent and not supposed to be effected by the M7.
Please advise on how the run of the M7 core effects the M4? nd what could be the reasons to my problem?