Question
switch from STM32f4 to stm32f7
Posted on October 06, 2015 at 15:13
Hello All
We have stm32f4 in a product running 168MHZ now switching to stm32f7 running At 168 MHz, the STM32F405/415 deliver 210 DMIPS/566 CoreMark performance executing from Flash memory, for stm32f7 ; At 216 MHz fCPU, the STM32F745 delivers 1082 CoreMark / 462 DMIPS performance executing from Flash I could not understand how much is the M7 is faster from M4 ; for example the same routine for both ; how much is it faster ? for a valid hardware and software ( M4) ; can we use for M7 ? Thank you in advanced