Skip to main content
denis
Associate III
September 6, 2013
Question

SVC_Handler fails badly - hardfaults

  • September 6, 2013
  • 10 replies
  • 2189 views
Posted on September 06, 2013 at 19:20

Below is the code for asm SVC handler straight from an example by ARM:

SVC_Handler

    STMFD        sp!,{r0-r3,r12,lr}          ; Store registers.

  LDR          r0,[lr, #4]                        ; Calculate address of SWI instruction and load it into r0.

    BIC          r0,r0,#0xff000000                ; Mask off top 8 bits of instruction to give SWI number.

    ;

    ; Use value in r0 to determine which SWI routine to execute.

    ;

    LDMFD        sp!, {r0-r12,pc}                    ; Restore registers and return.

  END                            ; Mark end of this file.

And i get Hard Fault failure on LDR instruction . wtf..  Any ideas?

I've seen same code sequence in many examples of the same SVC handler, and in other code.

    This topic has been closed for replies.

    10 replies

    Tesla DeLorean
    Guru
    September 6, 2013
    Posted on September 06, 2013 at 19:27

    What's the value in LR when it fails? I'd imagine it's a magic value indicating which stack was used? 0xFF??????

    The stack push/pop aren't balanced.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jpeacock2399
    Associate III
    September 6, 2013
    Posted on September 06, 2013 at 23:41

    Is the stack aligned to a word boundary?

      Jack Peacock
    denis
    denisAuthor
    Associate III
    September 9, 2013
    Posted on September 09, 2013 at 09:17

    >What's the value in LR when it fails? I'd imagine it's a magic value indicating which >stack was used? 0xFF??????

    Yes, the magic.

    >The stack push/pop aren't balanced.

    Yes, i see, copied wrong.  But thats not the problem (at that moment)

    denis
    denisAuthor
    Associate III
    September 9, 2013
    Posted on September 09, 2013 at 10:00

    Sorry i just correct a little my original post,  _but__ this is just because I was doing 4 things at same time, the copying to forum went wrong.

    name SVC_Handler

    public SVC_Handler

    section READONLY:CODE

    SVC_Handler

     STMFD        sp!,{r0-r3,r12,lr}   ; Store registers.

    LDR          r0,[lr, #-4]         ; Calculate address of SWI instruction and load it into r0.

    BIC          r0,r0,#0xff000000    ; Mask off top 8 bits of instruction to give SWI number.

    ; Use value in r0 to determine which SWI routine to execute.

    ;

      LDMFD        sp!, {r0-r3,r12,pc}^        ; Restore registers and return.

    END

    I'm puzzled with the instruction .

    LDR    r0,[lr, #-4] ; ; and yes its -4 for ARM not Thumb

    As clive1 pointed out, lr in when in SVC contains a magic value, the magic

    contained in only last 4 bits i think (saw in manual, can't recall page now..)

    So how is the above suppose to calculate the address of the SWI instruction

    and load it, that's magic to me. But i don't do ARM asm programming :\

    May be this does not apply to CortexM3 at all? I have not found a more

    CM3 specialized example..

    By the way,

    LDMFD   sp!, {r0-r3,r12,pc}^

    The ^ is 'kinda' important as i read, yet my asm compiler - IAR Systems -

    does not accept it..

    denis
    denisAuthor
    Associate III
    September 9, 2013
    Posted on September 09, 2013 at 10:03

    >Is the stack aligned to a word boundary?

    >  Jack Peacock

    Jack, now I do this right at start in my hal init:

    SCB->CCR |= SCB_CCR_STKALIGN;

    Still that SVC of mine promptly hard faults at same place ...

    denis
    denisAuthor
    Associate III
    September 9, 2013
    Posted on September 09, 2013 at 11:37

    clive1, and the magic in LR is

    0xFFFFFFF9.

    STM32F10xxx prog manual, p40: EXC_RETURN[3:0] = 0x09 = 0b1001.

     =

    ''Return to Thread mode.

    Exception return gets state from MSP.

    Execution uses MSP after return.''

    Do you know how that LDR instruction is suppose to do what the comment says it should ..?   Don't know if it explains the hardfault either ...

    Tesla DeLorean
    Guru
    September 9, 2013
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    denis
    denisAuthor
    Associate III
    September 9, 2013
    Posted on September 09, 2013 at 14:29

    Yea that's it... Pretty much same as my HardFault_Handler I copied else where, urghhg..

    Thanks

    denis
    denisAuthor
    Associate III
    September 9, 2013
    Posted on September 09, 2013 at 14:43

    void SVC_Handler(void)

    {

      __asm volatile(

        ''TST LR, #4      \n''

        ''ITE EQ          \n''

        ''MRSEQ R0, MSP   \n''

        ''MRSNE R0, PSP   \n''

        ''B svc_handler_c''

      );

    }

    void svc_handler_c (unsigned int * svc_args)

    { 

    // ...

     svc_number = ((char *)svc_args[6])[-2];

    // ....

    }

    thanks for pointed to that doc...
    Tesla DeLorean
    Guru
    September 29, 2015
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..