Skip to main content
RAdam.1
Associate III
January 8, 2026
Question

Supported PSRAM and Flash for the STM32N6xx

Hey guys,
 
I'm looking for some suitable HexaSPI PSRAM and also the OctoSPI Flash for the STM32N645 board I am just building.. I cant find the parts used on the DK so do you have a list of supported memories? I need 256Mb PSRAM and will start with a 1Gb Flash as per the DK.. 
 
Richard

5 replies

RomainR.
ST Employee
January 9, 2026

Hello @RAdam.1 

If you refer to the latest External Memory Manager Middleware,
STM32Cube_FW_N6_V1.3.0\Middlewares\ST\STM32_ExtMem_Manager\Release_Notes.html

You will find a list of NOR Flash SFDP from Winbond and Gigadevice manufacturer which are compatible with STM32N6.
Actually, concerning Hexa PSRAM/HyperRAM, only the APMemory APS256XXN-OBR-BG was validated on STM32N6.
After checking, it seems that the APS256XXN is available at Mouser.com.

APS256XXN-OBR-BG AP Memory - Distributors and Price Comparison | Octopart component search

Best regards,

Romain

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
January 13, 2026

It sounds like I'm in the same position as the original poster.

The recommended PSRAM APS256XXN-OBR-BG is showing as nearing the end of its lifecycle and not recommended for new designs. The manufacturer recommends APS256XXN-OB9-BG as a replacement.

Can anyone comment on the compatibility of APS256XXN-OB9-BG with the N6?

RomainR.
ST Employee
January 15, 2026

@johnchargo 

I reviewed the respective datasheets:

APS256XXN-OBRx – APM Octal PSRAM Datasheet, Rev. 1.00
APS256XXN-OBx9 – APM OPI/HPI Xccela PSRAM Datasheet, Rev. 1.2

The memory devices support the following serial interfaces with the Xcella support on OBx9 part number:
APS256XXN-OBRx: DDR Octal SPI
APS256XXN-OBx9: OPI/HPI and also supports Xccela™ mode for PSRAM

The main differences concern operating frequency and data rate:
APS256XXN-OBRx: Up to 200 MHz (400 MB/s in X8, 800 MB/s in X16)
APS256XXN-OBx9: Up to 250 MHz (500 MB/s in X8, 1000 MB/s in X16)

All other specifications listed below appear to be fully compatible:

Both part numbers are pin-to-pin compatible and share the same package dimensions.
Power-up initialization uses the same method and timing.
Address space, burst type and length, and command/address latching are identical.
The command truth table is the same.
Read operations use the same address/data transfer sequence and timing.
Write operations also appear to be aligned.

In my opinion, the APS256XXN-OBx9 should be compatible with STM32N6 XSPI without any modifications but limited to 200MHz with DQS.

Best regards.
Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Alex - APMemory
Associate II
February 4, 2026

Hi, 

Just to add few comment:  APS256XXN-OB9-BG - 256Mb is recommended latest device to use (APS512XXN-OB9-BG - 512Mb). This is latest version in production, fully compatible with STM32N6 (and other STM32 MCU supporting OPI). (APS256XXN-OBR-BG is the lower speed grade, not recommended for new design)

Thanks

Alex

RomainR.
ST Employee
February 4, 2026

Hi @Alex - APMemory 

Thank you to have confirmed the point.

Best regards,

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.