Skip to main content
NKieg.1
Associate III
Mar 19, 2021 9:34 AM UTC
Solved

Supplying voltage on VBAT pin on STM32F469I-DISCO

Hi everyone, I am currently working on a project working on a STM32F469I-DISCO. I would like to be able to use the embedded RTC as well as the backup SRAM. I have seen on the schematic that the VBAT pin is tied up to the 3.3V. Is there a way to still supply voltage to the VBAT pin (through the 3.3V for exemple) ?

Thank you.

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Mar 19, 2021 11:17 AM UTC

Looking at gerbers of rev.C, it appears that the VBAT track is on bottom, appears to be quite well accessible.

If this is a one-off and you have some skills with cutting/joining PCB tracks (i.e. the usual techniques used to fix botched prototypes which are otherwise OK), it could be cut and brought out to some suitable point.

JW

7 replies

waclawek.jan
Super User
Mar 19, 2021 10:48 AM UTC

Unfortunately, no.

The more dense DISCO boards are unfortunately not very well designed with respect to general usability. ST's strategy moved from DISCO boards as a vehicle for having joy through experimentation, towards Nuclei as barebone board, and Discos being shiny but single-purpose boards.

As I've said too many times, ST does not understand the reason of the STM32's success.

JW

NKieg.1
NKieg.1Author
Associate III
Mar 19, 2021 10:50 AM UTC

That's too bad ... My company wanted to avoid designing our own board but it may be something to think about then ...

waclawek.jan
waclawek.janBest answer
Super User
Mar 19, 2021 11:17 AM UTC

Looking at gerbers of rev.C, it appears that the VBAT track is on bottom, appears to be quite well accessible.

If this is a one-off and you have some skills with cutting/joining PCB tracks (i.e. the usual techniques used to fix botched prototypes which are otherwise OK), it could be cut and brought out to some suitable point.

JW

NKieg.1
NKieg.1Author
Associate III
Mar 19, 2021 11:49 AM UTC

Thank you a lot for your input. Unfortunately, this would not be a one off as we plan to use this board for a project which will be commercialized

Peter BENSCH
ST Technical Moderator
Mar 19, 2021 11:56 AM UTC

The use in a commercial product is not permitted anyway, see the Evaluation Board Terms Of Use:

The Evaluation Board shall not be, in any case, directly or indirectly assembled as a part in any production of Yours as it is solely developed to serve evaluation and testing purposes and has no direct function and is not a finished product.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.