Skip to main content
Senior
November 18, 2024
Solved

Stuck in Infinite_Loop

I am using the B-L072Z-LRWAN1 and trying to code LPTIM with interrupts and no HAL. The code seems to be getting stuck in the Infinite_Loop section in the startup.s file. The comments around this loop say that an unexpected interrupt was triggered. If I remove the NVIC functions in lptim_init(), the controller does not get stuck anymore. I have tried:

-setting the IER register to 127 (all interrupt sources enabled) with a breakpoint on the lptimer IRQ handler. The handler is never called.

-declared & defined all possible IRQ_Handler functions in stm32l0xx_it.c with a while(1) inside each one, and watched all of them with breakpoints. nothing.

-putting the NVIC functions before or after setting the IER register. no change.

here is my code for the lptimer:

 

void lptim_init(LPTIM_TypeDef *LPTIM, lpTimerMode mode)
{
	uint32_t tmpcfg = 0;
	uint16_t tmpier = 0;

	//enale the oscillator for the peripheral
	__HAL_RCC_LPTIM1_CLK_ENABLE();

	//encoder mode disabled
	tmpcfg &= ~LPTIM_CFGR_ENC;
	//counter mode disabled
	tmpcfg &= ~LPTIM_CFGR_COUNTMODE;
	//preload ARR
	tmpcfg |= LPTIM_CFGR_PRELOAD;
	//set wave polarity.
	tmpcfg &= ~LPTIM_CFGR_WAVPOL;
	tmpcfg &= ~LPTIM_CFGR_WAVE;
	//disable trigger event reset
	tmpcfg &= ~LPTIM_CFGR_TIMOUT;
	//disable hardware triggers
	tmpcfg &= ~LPTIM_CFGR_TRIGEN;
	//clear trigger selection
	tmpcfg &= ~LPTIM_CFGR_TRIGSEL;
	//set prescalar division
	tmpcfg |= LPTIM_PRESCALER_DIV1;
	//clear trig filter settings
	tmpcfg &= ~LPTIM_CFGR_TRGFLT;
	//external clock settings; clear.
	tmpcfg &= ~LPTIM_CFGR_CKFLT;
	//external source clock polarity. not relevant
	tmpcfg &= ~LPTIM_CFGR_CKPOL;
	//clock selection: internal clock
	tmpcfg &= ~LPTIM_CFGR_CKSEL;

	//write the configurations to the register
	LPTIM->CFGR = tmpcfg;

	//set interrupts to trigger on every ARR match
	if(mode == lptim_mode_interrupt)
	{
		//select the interrupt trigger sources
		tmpier |= LPTIM_IER_ARRMIE;
		//write the configurations to the register
		LPTIM->IER = tmpier;

		NVIC_SetVector(LPTIM1_IRQn, (uint32_t)&LPTIM1_IRQ_Handler);
		NVIC_SetPriority(LPTIM1_IRQn, 3);
		NVIC_EnableIRQ(LPTIM1_IRQn);
		//set the interrupt vector
	}
}

void lptim_start(LPTIM_TypeDef *LPTIM, uint16_t period)
{
	//enable the timer
	LPTIM->CR = LPTIM_CR_ENABLE;

	LPTIM->ARR = period;

	//enable continuous mode
	LPTIM->CR |= LPTIM_CR_CNTSTRT;
}

void lptim_stop(LPTIM_TypeDef *LPTIM)
{
	//clear control register, disabling the timer.
	LPTIM->CR &= ~0b111U;
}

 

 and in the main() and before while(1) I have

 

 lptim_init(LPTIM1, lptim_mode_interrupt);
 lptim_start(LPTIM1, LPTIMER_PERIOD);

 

 Does anyone know why this is?

This topic has been closed for replies.
gbm
gbmBest answer
Super User
November 18, 2024

There is no interrupt handler properly defined in your code, so the default handler is invoked.

NVIC_SetVector normally doesn't work - remove it.

Rename your interrupt routine to the name found in startup_xxx.s file - LPTIM1_IRQHandler.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

3 replies

gbm
gbmBest answer
Super User
November 18, 2024

There is no interrupt handler properly defined in your code, so the default handler is invoked.

NVIC_SetVector normally doesn't work - remove it.

Rename your interrupt routine to the name found in startup_xxx.s file - LPTIM1_IRQHandler.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Senior
November 19, 2024

Oh goodness. I've been staring at the code for too long and didn't notice that I wrote the IRQ handler function as LPTIM1_IRQ_Handler and not LPTIM1_IRQHandler. Thanks.

Tesla DeLorean
Guru
November 19, 2024

Should be LPTIM1_IRQHandler, check case

Do bisection of vectors in startup.s determine which ones make it to which infinite loop / Default_Handler

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..