Skip to main content
aamirali641989
Associate III
Jul 8, 2013 6:44 AM UTC
Question

Strange problem, sdhc card got intialized with debugger otherwise not

Posted on July 08, 2013 at 08:44

I have interface SDHC card with SPI protocol.

If I initialize the card while debugging it worked right. 

But if initialize it without it then card don't get initialized.

What could be the problem, like some timing issues. I also added 10ms delay b/w spi initialization & card initialization but didn't work.

Its timeout when I send CMD55_APP_CMD & ACMD41_SEND_OP_COND command
    This topic has been closed for replies.

    3 replies

    aamirali641989
    Associate III
    Jul 10, 2013 9:59 AM UTC
    Posted on July 10, 2013 at 11:59

    Any help on this. 

    frankmeyer9
    Associate III
    Jul 10, 2013 10:23 AM UTC
    Posted on July 10, 2013 at 12:23

    Hard to give a useful hint, without your hardware.

    I would add debug output, redirected to a uart, to find the difference.

    You could record the return values of the failing function calls, and compare with that seen during debugging.

    What could be the problem, like some timing issues.

     

    I suspect a timing problem, too.

    Have you tried lower bit rates ?

    Have you compared your implementation with other, working examples ?

    John F.
    Associate III
    Jul 10, 2013 10:42 AM UTC
    Posted on July 10, 2013 at 12:42

    Did you follow these steps?

    http://elm-chan.org/docs/mmc/mmc_e.html

    Chan's web site is usually very reliable.