Skip to main content
parisa
Associate III
Dec 26, 2016 5:26 PM UTC
Solved

Strange GPIOA output states

Posted on December 26, 2016 at 18:26

Hello,

Here is my code for set and reset PA.3 for stm32f10x

#include <stdio.h>

#include <string.h>

#include 'stm32f10x_gpio.h'

#include 'stm32f10x_rcc.h'

#include 'stm32f10x_tim.h'

void delay(void){

                int i,j;

        for(i=0;i<10000;i++)

        for(j=0;j<250;j++);

}

int main(void){

                GPIO_InitTypeDef GPStructure;

                RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA,ENABLE);

                GPStructure.GPIO_Mode=GPIO_Mode_Out_PP;

                GPStructure.GPIO_Pin=GPIO_Pin_3;

                GPStructure.GPIO_Speed=GPIO_Speed_50MHz;

                GPIO_Init(GPIOA,&GPStructure);

while(1){

GPIO_SetBits(GPIOA,GPIO_Pin_3);

delay();delay();delay();delay();delay();delay();

GPIO_ResetBits(GPIOA,GPIO_Pin_3);

delay();delay();

}

}

Well, I expect to get output voltage greater than 2.82 for high output voltage level and 0 for low voltage level but I get 1.3 for high output voltage level in set states! However it works fine for other ports (PB , ...)

In addition, I  test it for PA.15 but I get only 3.2 volt for set and reset!!!

what is my mistake?

    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Dec 26, 2016 7:09 PM UTC
    Posted on December 26, 2016 at 20:09

    Any details about the board you are testing this on?

    The most likely reason would be that the pin is connected to something else which is driving the pin low, and in the PA15 case could it be used by the debugger interface?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    3 replies

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Dec 26, 2016 7:09 PM UTC
    Posted on December 26, 2016 at 20:09

    Any details about the board you are testing this on?

    The most likely reason would be that the pin is connected to something else which is driving the pin low, and in the PA15 case could it be used by the debugger interface?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    parisa
    parisaAuthor
    Associate III
    Dec 26, 2016 9:14 PM UTC
    Posted on December 26, 2016 at 21:14

    Thanks dear Clive on , your are right.Another electrical component was driving the pin low.However the PA.15 is free and I don't use it. Should I deactivate a certain register?

    Tesla DeLorean
    Guru
    Dec 27, 2016 1:40 AM UTC
    Posted on December 27, 2016 at 01:40

    For the debug pins, you'd need remap the SWD/JTAG functionality off them. The Standard Peripheral Library v3.5.0 has a JTAG/GPIO example

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..