Stoping MDF (ADF) clock output
Greetings,
I'm using a low power microphone and would like to turn it off when not in use. That is done by turning off the clock to microphone, which is generated in ADF as output clock. Stopping sample acquisition (either by TRGO using window mode acquisition mode or by calling HAL_MDF_AcqStop()) does not stop the output clock. The only way I found to stop it is to call HAL_MDF_DeInit(), but that takes multiple clock cycles. Is there a way to set output clock to only be enabled when sampling? Also, when I DeInit the MDF, the clock pin stays High. Is there a way to leave it low (just pulldown resistor doesn't work)?