Skip to main content
CBald
Associate III
May 13, 2020 11:39 PM UTC
Solved

STOP2 mode scrambles stack on STM32L4R9

I'm really struggling with this problem. This is my first time trying to do anything low power, so please forgive any noob mistakes. All I'm trying to do is get the hang of a simple low power program so I can apply it to a larger one. My code is here: https://pastebin.com/zF5aPFGk

It's literally just about as simple as it can get, I've tried various combinations of commenting and uncommenting different functions (you'll notice some things like SYSCLKConfig_STOP(); commented out, but don't worry, it's been tried). It's just running on the 4MHz MSI default clock, with a 32.768kHz LSE connected to the RTC and LPUART

All the code should do is:

  1. turn on an LED
  2. print some text over UART
  3. wait 5sec
  4. turn off the LED
  5. print some more text
  6. go back to sleep.

Yet I kept getting random hardfaults. Eventually after days of debugging I've tracked it down to the stack becoming utter garbage as soon as it wakes up from STOP2 mode. Is there something I'm doing wrong here?

Stack before wfi instruction executes:

x/16xw $sp
0x2009ffc8:	0xc0ffffff	0x01000050	0x2009ffd8	0x2009ffd8
0x2009ffd8:	0xe000ed00	0x0000ffff	0x00000003	0x00000000
0x2009ffe8:	0x080001e5	0x0800550d	0x00000000	0x00000000
0x2009fff8:	0x00000000	0x08000c43	Cannot access memory at address 0x200a0000

Stack right as it enters the interrupt handler:

x/32xw $sp
0x2009ffa8:	0x00000001	0x00000001	0xe000ed00	0x00000001
0x2009ffb8:	0x00000000	0x080005f3	0x0800177e	0x61000000
0x2009ffc8:	0xe6513c6c	0xcae0959a	0x146f5b2a	0x33be356b
0x2009ffd8:	0x946b4f6f	0xeffaf2a7	0x64f8966b	0xcf7200b6
0x2009ffe8:	0x72fd85f8	0x7ff9767b	0x73b6792c	0x71f1f879
0x2009fff8:	0x1c961ccf	0xfcfbce38	Cannot access memory at address 0x200a0000

I'm also quite unsure how the stack is getting pushed up between the wfi and the first instruction of the interrupt handler, but if someone would like to look at the assembly or just knows why, I'd greatly appreciate it.

Assembly/list file is attached

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
May 14, 2020 9:12 AM UTC

RM0432 Rev 6 , 5.3 Low-power modes:

Stop 2 mode with SRAM3 content lost when the RRSTP bit is cleared in PWR_CR1 register (default setting).

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
May 14, 2020 9:12 AM UTC

RM0432 Rev 6 , 5.3 Low-power modes:

Stop 2 mode with SRAM3 content lost when the RRSTP bit is cleared in PWR_CR1 register (default setting).

JW

CBald
CBaldAuthor
Associate III
May 14, 2020 3:55 PM UTC

Thank you so much! I had been reading though RM0432, but missed that one part. Everywhere else (even a few lines above that quote) says that SRAM3 content is preserved in STOP2 mode. I should've looked harder! Thanks again :grinning_face: