Skip to main content
Anand A
Associate II
May 5, 2023
Question

Stop flag is not generated with STM32H743BI manually written i2c driver.

  • May 5, 2023
  • 2 replies
  • 860 views

Hello,

I am trying to write manual I2C driver for STM32H743BI controller. Here system clock is configured for 200MHz and APB1 clock for 50MHz. Below is my initialization code. While testing stop flag and TXIS flag is not set after setting CR2 register. Is there anything I am missing here?

Slave address is 0xA0 (EEPROM).

RCC->APB1LENR |= RCC_APB1LENR_I2C1EN;

RCC->AHB4ENR |= RCC_AHB4ENR_GPIOBEN;

 GPIOB->MODER &= 0xFFFFAFFF;

 GPIOB->OSPEEDR &= ~0x0000F000;

 GPIOB->OTYPER |= 0x000000C0;

 GPIOB->PUPDR |= 0x00005000;

 GPIOB->AFR[0] |= 0x44000000;

 GPIOB->AFR[1] = 0x00000000;

 I2C1->CR1 = 0x00000000;

 I2C1->TIMINGR = 0x00901954;

 I2C1->CR1 = 0x00000001;

 I2C1->CR2 = 0x02000000;

 I2C1->OAR1 = 0x00008000;

 I2C1->OAR2 = 0x00000000;

 // Check Slave Ready

 I2C1->CR2 = 0x020000A0; // Address 0xA0

 while((!(I2C1->ISR & I2C_ISR_STOPF)) && (!(I2C1->ISR & I2C_ISR_NACKF)));

 if((I2C1->ISR & I2C_ISR_NACKF) == 0)

 {

   I2C1->ICR |= I2C_ICR_STOPCF;

 }

 // Transfer Addr

 I2C1->CR2 = 0x010200A0;

 // Wait unitil TXI flag is set.

 while(!(I2C1->ISR & I2C_ISR_TXIS));

 I2C1->TXDR = 0xB0;

 while(!(I2C1->ISR & I2C_ISR_TXIS));

 I2C1->TXDR = 0x00;

 while(!(I2C1->ISR & I2C_ISR_TCR));

 // Transfer Data

 I2C1->CR2 = 0x020200A0;

 while(!(I2C1->ISR & I2C_ISR_TXIS));

 I2C1->TXDR = 0x55;

 while(!(I2C1->ISR & I2C_ISR_TXIS));

 I2C1->TXDR = 0xAA;

 while(!(I2C1->ISR & I2C_ISR_TXIS));

 while(!(I2C1->ISR & I2C_ISR_TCR));

 while(!(I2C1->ISR & I2C_ISR_STOPF));

 I2C1->ICR |= I2C_ICR_STOPCF;

 // to Read

   // Transfer Addr

 I2C1->CR2 = 0x000200A0;

 // Wait unitil TXI flag is set.

 while(!(I2C1->ISR & I2C_ISR_TXIS));

 I2C1->TXDR = 0xB0;

 while(!(I2C1->ISR & I2C_ISR_TXIS));

 I2C1->TXDR = 0x00;

 while(!(I2C1->ISR & I2C_ISR_TC));

 I2C1->CR2 = 0x020204A0;

 while(!(I2C1->ISR & I2C_ISR_RXNE));

 data[0] = I2C1->RXDR;

   while(!(I2C1->ISR & I2C_ISR_RXNE));

 data[1] = I2C1->RXDR;

   while(!(I2C1->ISR & I2C_ISR_TCR));

 while(!(I2C1->ISR & I2C_ISR_STOPF));

 I2C1->ICR |= I2C_ICR_STOPCF;

 //ClearI2C Reg

 I2C1->CR2 = 0x02000000;

 while(1);

This topic has been closed for replies.

2 replies

Joe WILLIAMS
ST Employee
May 9, 2023

Hi Anand A

Your question has been routed to the online support team. A case has been created and you'll be contacted shortly.

Kind Regards

Joe WILLIAMS

STMicro Support

Piranha
Principal III
May 10, 2023

Why are you using the register bit field definitions only for status registers, but not for configuration registers? And does this code even correspond to the I2C state machine described in the reference manual?