Skip to main content
mnemxys
Associate II
July 3, 2015
Question

Stop code execution during 8 timer interrupts

  • July 3, 2015
  • 2 replies
  • 694 views
Posted on July 03, 2015 at 14:14

Hi everyone,

I'm working with the stm32f405 microcontroller and I am trying to send some characters using a simple GPIO pin. My problem is that I have to send each bit of one character every 20ms. For that I use a timer interruption. In this case, every 8 executions of the interrupt I will have sent a complete character and I can start sending the next one.

The problem is that I have to wait until 8 interruptions have execute or the code continues executing between interruptions and the character value will change. Therefore, I would need to stop the code durint 8 interruptions. To do that, I use a counter into the interruption and a while(counter < 8); in my main code but nothing happens. The code executes entirelly before the interrupts and only can send the last character.

What could I do to stop the code during 8 interruptions?

I hope you can help me. Thank you very much in advance.

Regards!!

mnemxys

 
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    July 3, 2015
    Posted on July 03, 2015 at 15:58

    Couldn't you just buffer the data properly so this doesn't happen?

    Have the interrupt pull it's OWN copy of the data every 8 cycles, and have a FIFO (Ring) Buffer hold the subsequent character(s). Have the filling side check if it's FULL, and spin in a loop until the interrupt frees up space.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    mnemxys
    mnemxysAuthor
    Associate II
    July 10, 2015
    Posted on July 10, 2015 at 16:20

    Oh, Clive1, I forgot to answer you. I finally did as you adviced me and now I have my code working smoothly although I'm having other problems, but that's another story.

    Thank you very much for your help.

    mnem