Skip to main content
pt1
Associate III
May 6, 2009
Question

STOne-32 - where is the pc tool for the boot loader

  • May 6, 2009
  • 3 replies
  • 750 views
Posted on May 06, 2009 at 06:27

STOne-32 - where is the pc tool for the boot loader

    This topic has been closed for replies.

    3 replies

    pt1
    pt1Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:11

    Hi STOne-32,

    you wrote 2007 that you will soon have a tool for downloading firmware via the boot loader located the system memory of the STM32F10x. I want to use the USART1. Do you have the tool already? I can't find it - please help.

    I've tried several terminal programs but no one would be sufficient.

    By the way it is a great problem to send the 2 bytes for a command. It is easy to send 2 bytes direct one after the other. But that produces a NACK. If I send the 2 bytes with a timeout then I'll get a respond. But it is very difficult to send a ACK then. The way it works seems to be only useful with your tool, or not?

    Best regards pt1

    [ This message was edited by: pt1 on 05-05-2009 18:58 ]

    pt1
    pt1Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:11

    Hi STOne-32,

    you are my ''One'' and only :D . Thank you very much.

    Best regards pt1

    16-32micros
    Associate III
    May 17, 2011