Skip to main content
tobias2399
Visitor II
March 13, 2013
Question

STMStudio 3.1.1 does not show all variables on import

  • March 13, 2013
  • 2 replies
  • 891 views
Posted on March 13, 2013 at 11:57

Hi,

after I updated the STMStudio I'm not able to import all variables from the .efl file.

After selecting a file there are not all variables shown. I tried different toolchains, but the problem is still there.

I use an old config (I think it was created with STMStudio 2.x or something) and my charts and variables are working.

I can also add new variables to the ''Display Variables settings'' but I must do this by hand:

1. Right click ''new'', rename it  to my variable name

2. Looking for the address of the variable in .map file or disassembled source.

2. Set the corect address and type.

Now I can use it as before for example in graphs or tables.

I'm not sure if I did something wrong, but the variables are present in .map and also in .elf file (checked with an text editor).

Has somebody a suggestion for me?

Thanks and greets

Tobias
    This topic has been closed for replies.

    2 replies

    v239955_st
    Visitor II
    June 28, 2013
    Posted on June 28, 2013 at 11:48

    Hi!

    I recognize your problem; I also couldn't find the variable I was looking for in the list, and had to find the address in the map file. Even worse, this was a struct, so I had to manually enter all adresses. Even being able to use offsets would have been a nice feature (using expressions in the Address field), or using reference / dereference operators....

    S C
    ST Employee
    July 1, 2013
    Posted on July 01, 2013 at 13:26

    Hello,

    May you please precise with which toolset (compiler) version the elf file was made, and also give an example how such missing variables were defined in source files.

    Using basic types in variable definition should avoid any potential issue (even for structure fields).

    Moreover, bitfields and multi-dimensional tables are not managed by the STMStudio symbol browser.

    Thank you