Skip to main content
stcom9174
Associate III
September 8, 2016
Question

STM7 - PWM in LP Mode(s)

  • September 8, 2016
  • 3 replies
  • 693 views
Posted on September 08, 2016 at 13:15

Hello All,

Is it possible for the STM7x family to drive PWM outputs - specifically here TIM1 and TIM8 - in Low Power Mode?

Thanks,

John W.

#stmf7-lp-pwm
This topic has been closed for replies.

3 replies

slimen
Visitor II
September 8, 2016
Posted on September 08, 2016 at 15:43

Hi,

Yes, It is possible to drive PWM outputs.

You can refer to the

http://http://www.st.com/content/ccc/resource/technical/document/reference_manual/group0/96/8b/0d/ec/16/22/43/71/DM00224583/files/DM00224583.pdf/jcr:content/translations/en.DM00224583.pdf

for more details and section ''25 Advanced-control timers (TIM1/TIM8)''.

Regards

stcom9174
stcom9174Author
Associate III
September 9, 2016
Posted on September 09, 2016 at 09:24

Yes, and, where, specifically, is the discussion about running PWM in low power mode?

I see in chapter 29 - the LPTIM can be run in PWM mode; but what about TIM1/TIM8?

Hence the original question.  

Thanks,

John W.

waclawek.jan
Super User
September 9, 2016
Posted on September 09, 2016 at 10:37

Specify ''low power mode'' first.

As long as there is power and clock supplied to timers, they work. There is nothing ''low-power-specific'' in the PWM modes of Timer.

Review Table 12. Low-power mode summary in RM0385 rev.2. Note the RCC_APBxLPENR registers in RCC.

JW