Skip to main content
raptorhal2
Lead
July 2, 2014
Question

STM42F4 Pin 1 Identifier

  • July 2, 2014
  • 7 replies
  • 4686 views
Posted on July 02, 2014 at 02:49

Just received some STM32F405RGT6 (64 pin LQFP) processors with two round circles on opposite corners of the package, one smaller with a concave bottom, the other larger with a flat bottom. The package description in the datasheet of course shows only one mark. Can anyone tell me which is the real Pin 1 identifier ? I suspect it is the smaller circle, but I don't want to risk letting all the smoke out of the chip finding out.

The F405 144 pin LQFP processors also just received correctly have only one pin marker.

Thanks, Hal

 
    This topic has been closed for replies.

    7 replies

    Tesla DeLorean
    Guru
    July 2, 2014

    Posted on July 02, 2014 at 02:52

    https://community.st.com/t5/stm32-mcu-products/stm32f401-64pin-pin1-marking-orientation/m-p/419306

    https://community.st.com/0D50X00009Xka68SAB now dead

    Edit: Fixed DEAD LINK, original post from 1-July-2014, fixed again

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Visitor II
    August 17, 2023

    Link above is bad.
    Solved: Ambiguity in pin-1 position on stm32f756vgt6 - STMicroelectronics Community
    Seems Pin 1 is lower left when the ST text is properly oriented for reading

    raptorhal2
    Lead
    July 2, 2014
    Posted on July 02, 2014 at 03:32

    Thanks, Clive1. Hal

    Tesla DeLorean
    Guru
    August 17, 2023

    Yes, every time they migrate the forum content gets lost or destroyed. I'll flag this.

    @Amelie ACKERMANN can you get this checked/fixed. Thread would likely have been one showing multiple pin count packages with molding and orientation markings identified.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Amelie ACKERMANN
    ST Community Manager
    August 18, 2023

    Hello @Tesla DeLorean,

    is this the correct thread? STM32F401 64pin pin1 marking / orientation - STMicroelectronics Community
    If so, it is now moved to the "STM32 MCU products" forum board. If not, let me know and I can check further. 

    Thanks,
    Amelie

    Andrei Chichak
    Lead
    August 24, 2023

    Also, note that the orientation indicated in CubeMX and CubeIDE is wrong with respect to the lettering on the processor.

    I reported this a while back, but what can you do?