Skip to main content
gazam
Visitor II
March 4, 2016
Solved

stm3f373 clock and flash latency setting

  • March 4, 2016
  • 1 reply
  • 888 views
Posted on March 04, 2016 at 09:19

I worked with stm32f373.

To reduce power consumption I change the Hclk to 24Mhz and 48Mhz System clock.

(use AHB prescaler to /2)

But I confused by flash setting.

reference manual said that the latency is

000: Zero wait state, if 0 < SYSCLK? 24 MHz

001: One wait state, if 24 MHz < SYSCLK ? 48 MHz

010: Two wait sates, if 48 < SYSCLK ? 72 MHz

but the st library source code said that the latency is choosed by Hclk  not system clock

what is correct?

and what should I consider when the sys clk different with Hclk ?

#stm32
    This topic has been closed for replies.
    Best answer by Amel NASRI
    Posted on March 04, 2016 at 15:21

    Hi choi.gazam,

    The number of wait states depends on HCLK range.

    The description should be reviewed in the reference manual. 

    Thanks for highlighting this.

    -Mayla-

    1 reply

    Amel NASRI
    Amel NASRIBest answer
    ST Technical Moderator
    March 4, 2016
    Posted on March 04, 2016 at 15:21

    Hi choi.gazam,

    The number of wait states depends on HCLK range.

    The description should be reviewed in the reference manual. 

    Thanks for highlighting this.

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.