Skip to main content
Associate II
July 2, 2026
Question

stm32wb does not run when power on

  • July 2, 2026
  • 0 replies
  • 4 views

Hello ST Community,

I am working with STM32WB05 in a custom PCB (new design) and it does not run when power on the PCB. To run it, I have to reset by reset line. If I am debugging, I neither have problem.

I had used others microcontroller before (STM32L1, STM32WL55...) and it had never happend.

 

I have check the pollowing points:

1-  Power supply. I am using a externa battery with 3-3,5Volts.

2- BOOT pin: I think that the problem is the STM32WB05 enter in boot mode but in the datasheet, I can not see any pin to enter it.

I have tried to join PA10 to GND by 10K resistor (I see in nucleo manual UM3343 that BOOT0 pin is PA10) but that no work.

3-  Clock source: I am using interna clock HSE

4- reset line is always high level

 

Any confirmation or guidance would be greatly appreciated.

Thank you for your support.