Question
STM32VL / STM32F4 Discovery working with ethernet
Posted on January 21, 2013 at 03:48
Hi Great people of STM32,
I would like to ask if it is possible to work with lan directly with the MCU or I need to buy interface shields that communicate via spi? but i have seen that stm32 has dedicated pins for ethernet and you can configure sram for it means it can have buffers when that happen can I pipeline on those two rams ram for gpio and ram for ethernet so those two execute simultaneously?