Skip to main content
peppea82
Associate II
Nov 2, 2012 6:54 AM UTC
Question

STM32VL Discovery and I2C Accelerometer

Posted on November 02, 2012 at 07:54

I need some help setting up I2C connection to LIS302DL or a generic I2C accelerometer. I need some code examples to get the accelerometer working. Thanks in advance.

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    Nov 2, 2012 10:13 AM UTC
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    peppea82
    peppea82Author
    Associate II
    Nov 2, 2012 11:00 AM UTC
    Posted on November 02, 2012 at 12:00

    Sorry but I think iNemo is unrelated. I'll try to explain better.

    I have an STM32VLDiscovery board and a LIS302DL accelerometer. They are connected using i2c to the stm32vl discovery.

    LIS302DL is provided in an adapter board where I connected

    LIS side -> STM32VL side

    VDD -> 3v3

    CS -> 3v3

    SCL -> PB6

    SDx -> PB7

    SDO -> 3v3

    GND -> GND

    I have to accomplish a very simple task: get data from i2c and put data to usart.

    I2C is initialized using the following code:

    static void I2C1_GPIO_Config(void)

    {

      RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);

      RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);

      GPIO_InitTypeDef GPIO_InitStructure;

      I2C_InitTypeDef I2C_InitStructure;

      GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;

      GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_OD;

      GPIO_Init(GPIOB, &GPIO_InitStructure);

      I2C_Cmd(I2C1, ENABLE);

      I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;

      I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;

      I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

      I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

      I2C_InitStructure.I2C_ClockSpeed = 100000;

      I2C_InitStructure.I2C_OwnAddress1 = 0;

      I2C_Init(I2C1, &I2C_InitStructure);

    }

    Read from i2c is done by

    I2C_GenerateSTART(I2C1, ENABLE);

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));

    I2C_Send7bitAddress(I2C1, 0x1d, I2C_Direction_Transmitter);

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));

    I2C_SendData(I2C1, 0x20);

    while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

    I2C_GenerateSTART(I2C1, ENABLE);

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));

    I2C_Send7bitAddress(I2C1, 0x3B, I2C_Direction_Receiver);

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED));

    data = I2C_ReceiveData(I2C1);

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED));

    I2C_GenerateSTOP(I2C1, ENABLE);

    I'm using Atollic free version.

    Code gets stuck on

    while(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));