Skip to main content
luisfynn1
Associate II
Apr 16, 2026 6:02 AM UTC
Question

STM32U5G9 HSPI1: Only 2 of 4 QSPI data lines active during pixel write

Only 2 of 4 QSPI data lines active during pixel write, despite DMODE=3 confirmed in CCR

 

이미지 4장을 모두 참조하여 ST Community 문의 글을 작성합니다.

Environment

  • MCU: STM32U5G9ZJ (Cortex-M33, TrustZone enabled)
  • IDE: STM32CubeIDE
  • HAL version: STM32U5xx HAL Driver (included in project)
  • Interface: HSPI1 → QSPI LCD (ICNA3306-compatible controller)

 

Hardware Configuration

GPIO settings are shown in [XSPI_2.png]. All six HSPI1 pins are configured as Alternate Function Push-Pull with GPIO_SPEED_FREQ_VERY_HIGH and GPIO_AF8_HSPI1:

Pin Signal Speed
PI3 HSPI1_CLK Very High
PH9 HSPI1_NCS Very High
PH10 HSPI1_IO0 Very High
PH11 HSPI1_IO1 Very High
PH12 HSPI1_IO2 Very High
PH13 HSPI1_IO3 Very High

Clock configuration is shown in [XSPI_3.png]: HSPI1 kernel clock source is set to SYSCLK (160 MHz). PLL1: HSE(16MHz) × PLLN(10) / PLLR(1) = 160 MHz.

CubeMX parameter settings are shown in [XSPI_1.png]:

  • Fifo Threshold: 4 bytes
  • Memory Type: Micron
  • Clock Prescaler: 1 (→ FCLK = 80 MHz)
  • Clock Mode: Low (Mode 0)
  • Sample Shifting: Half Cycle

 

Problem Description

I am trying to write a full-frame image (194×368, RGB565 = 142,784 bytes) to the LCD using HSPI1 in indirect write mode with 4-line data (quad SPI).

The pixel write command uses instruction 0x32 with a 24-bit address 0x002C00 (encoding the RAMWR command 0x2C), and DataMode = HAL_XSPI_DATA_4_LINES, as shown:

sCommand.InstructionMode = HAL_XSPI_INSTRUCTION_1_LINE;
sCommand.Instruction = 0x32;
sCommand.AddressMode = HAL_XSPI_ADDRESS_1_LINE;
sCommand.AddressWidth = HAL_XSPI_ADDRESS_24_BITS;
sCommand.Address = 0x002C00;
sCommand.DataMode = HAL_XSPI_DATA_4_LINES; // ← intended quad
sCommand.DataLength = totalBytes; // 142784
sCommand.DummyCycles = 0;
sCommand.DQSMode = HAL_XSPI_DQS_DISABLE;
sCommand.SIOOMode = HAL_XSPI_SIOO_INST_EVERY_CMD;

Oscilloscope measurement shows that only IO0 and IO1 carry data. IO2 and IO3 remain at constant levels (IO2 = constant LOW, IO3 = constant LOW) throughout the entire data phase.

 

What I Have Verified

I read the HSPI1->CCR register immediately after HAL_XSPI_Command() returns and confirmed:

HSPI1->CCR = 0x03002101

Breakdown:
 bits [2:0] = 001 → IMODE = 1-LINE ✓
 bits [10:8] = 001 → ADMODE = 1-LINE ✓
 bits [13:12] = 10 → ADSIZE = 24-bit ✓
 bits [26:24] = 011 → DMODE = 4-LINES ✓
 bit [30] = 0 → SIOO = INST_EVERY_CMD ✓

DMODE is confirmed as 3 (quad) in the hardware register. The STM32 HSPI peripheral should therefore be driving all four IO pins as outputs during the data phase. However, the oscilloscope consistently shows only IO0 and IO1 toggling.

I also verified:

  • All HSPI GPIO pins are physically connected to the LCD (PCB continuity confirmed)
  • LCD is initialized with 0xC4 = 0x80 to enable DSPI mode before the pixel write
  • HAL_XSPI_Command() returns HAL_OK
  • Image buffer is 4-byte aligned and located in SRAM (static variable)

Questions

  1. If DMODE = 3 (quad) is confirmed in HSPI_CCR, is it possible for the HSPI peripheral to still output only 2 data lines? Is there any other register (e.g., MSEL in CR, or a DLL calibration state) that could gate IO2/IO3?

  2. The LCD is initialized with 0xC4 = 0x80 ("DSPI mode enable" per the LCD vendor's initialization sequence). Could this register value be enabling only 2-wire (dual) mode on the LCD side, causing IO2/IO3 to be driven to fixed levels by the LCD controller and contending with the STM32? If so, what value of 0xC4 enables true 4-wire (quad) mode?

  3. In indirect write mode (FMODE=00) with ADMODE≠0 and DMODE≠0, RM0456 states that the transfer is triggered by the first write to HSPI_DR — not HSPI_AR. Is this correct? If so, does the FTF flag in HSPI_SR behave normally (set when FIFO has free space) before the first DR write, or is FTF only meaningful after the transfer has been triggered?

Any guidance would be greatly appreciated. Thank you.

3 replies

Ghofrane GSOURI
ST Technical Moderator
Apr 16, 2026 7:55 AM UTC

Hello @luisfynn1 

Thank you for posting.

Could you please share  [XSPI_3.png],  [XSPI_2.png] and  [XSPI_1.png] ?

In meantime , I will try to reproduce your case based on your description. I will get back to you ASAP. 

 

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
luisfynn1
luisfynn1Author
Associate II
Apr 16, 2026 10:35 PM UTC

..

Ghofrane GSOURI
ST Technical Moderator
Apr 21, 2026 11:58 AM UTC

Hello @luisfynn1 

Regarding your first question :

HSPI_CCR.DMODE = 0b011 confirms that the STM32U5 HSPI peripheral is configured for a 4-line data phase ( 4 bits at a time (over IO0 to IO3 in quad-SPI mode)), and under normal documented operation it should drive IO0 to IO3 during that phase.

GhofraneGSOURI_0-1776772206322.png

My understanding that there is no typical hidden STM32 mechanism, such as MSEL in CR or DLL calibration state, that would silently downgrade a configured quad transfer into dual output while DMODE still reports quad.

I am forwarding your question to the appropriate team so you can receive more efficient support.

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.