Solved
STM32U5A9J-DK1 USB Device as mass storage standalone via sdmm1 emmc
- 10 replies
- 1621 views
I want to use the EMMC as USB storage space, but I encountered another issue: I am trying to access the EMMC via SDMM1, and after implementing the MSC-related functions (read, write, USBD_STORAGE_GetMediaLastLba, USBD_STORAGE_GetMediaBlocklength) in ux_device_msc.c, the formatting operation on the PC side fails. The error message says: "Please insert a disk into the removable disk."
I have already verified that after initializing SDMM1, the EMMC can be accessed and read/write operations are successful.
What could be the reason for this issue?
The attached file is my project.

ux_device_msc.c: