Skip to main content
Associate III
December 23, 2024
Question

STM32U5A5QJI6Q - Which Pins to Use for Programming ?

  • December 23, 2024
  • 4 replies
  • 718 views

Hi,

I am working with the STM32U5A5QJI6Q microcontroller and need guidance on the programming pins. I plan to program it using [SWD/JTAG (choose one)] with an external programmer like ST-Link.

Could someone confirm:

  1. Which pins are used for programming via [SWD/JTAG]?
  2. Are there any specific configurations or settings I need to enable in the hardware or firmware for successful programming?
  3. If using the internal bootloader, what are the required connections (e.g., UART or USB pins)?

I am currently working on a project that incorporates the STM32U5A5QJI6Q microcontroller, and I would like to request the official reference design or any relevant design resources for this specific part. Having access to a detailed reference design would greatly assist in ensuring an optimal hardware implementation.

Any reference to the datasheet or specific examples would be greatly appreciated.

Thank you!

Sathiya

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
December 23, 2024

For SWD, minimally PA13/PA14, read the Data Sheet

For System Loader options, review Application Note AN2606

For a Schematic, go to the "CAD Resources" tab for NUCLEO, DISCO, or EVAL boards

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate III
December 23, 2024

Hi send me the link For a Schematic, go to the "CAD Resources" tab for NUCLEO, DISCO, or EVAL boards.

TDK
December 23, 2024
"If you feel a post has answered your question, please click ""Accept as Solution""."