Skip to main content
Associate III
October 23, 2024
Question

STM32U5A5QJ Part Selection Clarification

Hi,

We are currently in the process of selecting components for our project, and we have identified the STM32U5A5QJ9 (STM32U5A5QJ), foot-print size UFBGA 132 7x7x0.6 P 0.5 mm) microcontroller as a potential candidate. However, upon reviewing the datasheet, we noticed that there are two variants available: one with SMPS (Switched-Mode Power Supply) and one without.

Could you please provide clarification on the differences between these two variants? Specifically, we would like to understand the functionality and features that differentiate the STM32U5A5QJ variant with SMPS from the one without SMPS.

 

Additionally, as we are interested in procuring the exact variant that suits our project requirements, could you please advise on how we can accurately specify and order the desired variant online?

Which variant is suitable for a wearable device (battery powered)?

 

Regards,

Sathiya

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
October 23, 2024
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.