STM32U5A5 USB Device Only Question
- 6 replies
- 889 views
Hi, I'm seeking some advice on using a STM32U5A5 in USB device only via a USBC connection.
Any previous USB "device only" designs I've worked on only required connections to D+, D- and ground to communicate. These designs have been USB2x.
The U5A5 has lots of cool features regarding the USB module etc but we have assigned other features to the pins that are associated with the more the more advanced features like CCx and VBUS SENSE etc. As we plan to use the part in device only mode am I correct in assuming that reallocating the unused pins OK to do and that D+, D- and GND are the only connections required?
We are using the USBC port for a communications link to a PC using CDC, and developing with the associated NUCLEO-U5A5ZJ-Q board. However our product schematic will look like the one in the attached schematic snippet.
Thanks in advance
Caleb