Skip to main content
Associate II
Jun 18, 2025 3:31 AM UTC
Question

STM32U585x ADC Differential and Single-Ended Channel Configuration

Hi ST Community Team,

I am currently working with the STM32U585x SoC family and need assistance with configuring the ADC for multiple channels. My project involves:

  1. One differential input signal using PA0 and PA1 (Channel 5)

  2. Six single-ended input channels: CH7, CH8, CH9, CH10, CH11, and CH12

Could you please guide me on the following:

  1. How can I read data with high precision for the differential signal (PA0 and PA1, CH5)?

  2. How can I read data from the single-ended channels listed above?

I would appreciate your help in configuring both types of signals in a single project, Please share the STM32 Cube configurations and Firmware of it.

Thank you in advance for your support.

This topic has been closed for replies.

2 replies

TDK
Jun 18, 2025 12:36 PM UTC

This should be fairly trivial to set up in CubeMX. Have you tried? Have you gotten the ADC to work in a project at all?

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Employee
Jun 18, 2025 4:02 PM UTC

Hi @ram_jana 

As mentioned by @TDK, with CubeMX, you should be able to set CH5 to differential mode (the corresponding negative channel will be automatically locked.)

You can check this FW example including .ioc file: STM32CubeU5 Projects NUCLEO-U575ZI-Q Examples ADC /ADC_DifferentialMode

 

Hope that helps! 
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.