Skip to main content
CWeav.1
Associate
November 17, 2022
Question

STM32U585 SPI Transmit issue: Partial last byte transmitted

  • November 17, 2022
  • 4 replies
  • 1786 views

Hardware: B-U585I-IOT02A dev kit

SPI1 configuration:

  • Master mode
  • 8-bit data size
  • NSS hard output
  • Tx only (2-lines)
  • MSB first
  • PCLK: 160 MHz; Baud Prescaler 32 yields SPI sck of 5MHz
  • no CRC
  • fifo threshold 1-data
  • Master Keep IO State enabled
  • RDY management internal (ie RDY disabled)

When running long-term reliability tests between 2 devkits, we occasionally will detect a transmission error which has been determined to be due to missing the final byte of the transfer. When viewed on a scope, only the first 3 SCKs are provided for the final byte then the transfer is ended (NSS goes high immediately after the 3rd SCK). This occurs when using HAL_SPI_Transmit(). Even when decoupling the NSS signal from SPI hardware control and driving it manually with software, the failure always presents itself as the Tx only shifting the first 3 bits of the last byte. We have tried slower and faster SCK baud prescalers with the same result. I would note that this problem occurs after many hundreds of thousands of successful transfers and always on the final byte of the transfer.

Looking for any ideas of what could be going on as it is unclear from the reference manual what could cause a transfer to end abruptly like this. The errata does not have any notes which seem to be related to this. It is not easy to post actual example code but the SPI driver code is highly modeled after Cube example code provided. But happy to provide any other information that might be relevant.

Thanks in advance for any help!

This topic has been closed for replies.

4 replies

S.Ma
Principal
November 18, 2022

Yoy are sure all databit have been sent out when RXNE is set. Not the TXE.

CWeav.1
CWeav.1Author
Associate
November 18, 2022

Thanks for the reply. I believe those are I2C peripheral flags, not SPI for the U585 part.

gbm
Super User
November 18, 2022

It's not about beliefs, Read The Fine Reference Manual.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
S.Ma
Principal
November 19, 2022

An SPI data transfer is known to be full completion when the received data truggers interrupt. Avoid using data trannsmit interrupt.