Skip to main content
ASavi.3
Associate II
November 24, 2023
Question

STM32U585 - Problem with more than one wake up pin in Stop3 mode

  • November 24, 2023
  • 4 replies
  • 1517 views

Dear all,

I am using STM32U585CIT6Q in Stop3 mode. When one wakeup pin is active, everything works fine, and I can wake up my microcontroller.

But when I want to use two wakeup pins (Two wakeup pins are selected in .ioc file and enabled in code), I can't wake up the microcontroller.

What could be a problem?

Best regards,

Ana

This topic has been closed for replies.

4 replies

Visitor II
November 24, 2023

Please check if the pins are configured with the appropriate triggering sensitivity (e.g., rising edge, falling edge, etc.).

ASavi.3
ASavi.3Author
Associate II
November 24, 2023

I don't think that is the problem. The wakeup pins are enabled with functions:

HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4_LOW_0);

HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN6_LOW_0);

That means that wakeup pins have a low polarity.

When I use one or the other of these wakeup pins, everything works as it should.

Best regards,

Ana

ST Employee
November 24, 2023

Hello @ASavi.3

What pins are you using as wakeup pins?

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ASavi.3
ASavi.3Author
Associate II
November 24, 2023

Hello @Sarra.S ,

I'm using PA2 and PB5