Skip to main content
Associate
May 16, 2025
Question

STM32U575ZIT6 USB FS problem

  • May 16, 2025
  • 2 replies
  • 328 views

Hello all, i got a firmware configuration problem,

 

basically im using USB in FS modem and when i plug in the usb to  the pc what happens is that sometimes it can be recognized and i see a network disk called ''boot'' but most of times it cant be recognized, so i gotta power up again the whole circuit until it can be seen, i thought it would be a frequency problem, but i already saw that configuration is set to 48MHz , so its correct, i added also a delay before initialization of the usb but it still doesnt work, what else i can try? can someone give me some tips? i already read on many forums but still didnt find out

This topic has been closed for replies.

2 replies

ST Technical Moderator
May 16, 2025

Hi @USER291279641 
Would you attach screenshot of USB Device manager?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate
May 16, 2025

i found out, i was using internal oscillator at 48MHz, which isnt precise.

 

Now im using the one at 8MHz+PLL and it works fine