Skip to main content
Adriano Melis
Associate III
February 21, 2024
Solved

STM32U575VGT HAL_FLASHEx_Erase() not working (page is not erased)

Hello all,

this code snippet is not working: the page is not erased, although the HAL does not report errors.

No RTOS is running.

 

if (HAL_ICACHE_Disable() != HAL_OK) {

Error_Handler();

}

 

status = HAL_FLASH_Unlock();

if (status != HAL_OK) {

Error_Handler();

}

 

erase_init_struct.TypeErase = FLASH_TYPEERASE_PAGES;

erase_init_struct.Banks = FLASH_BANK_1;

erase_init_struct.Page = 127;

erase_init_struct.NbPages = 1;

 

status = HAL_FLASHEx_Erase(&erase_init_struct, &page_error);

if (status != HAL_OK) {

Error_Handler();

}

 

Any suggestion?

 

 

 

This topic has been closed for replies.
Adriano Melis
Adriano MelisBest answer
Associate III
February 23, 2024

Hello all,

I found the source of the problem: the DUALBANK bit in FLASH_OPTR was set to 1.

On this device this arranges the FLASH page access in two banks of 64 pages each.

 

12 replies

TDK
February 21, 2024

How are you verifying the page is not erased? What tool and memory addresses are you looking at?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Adriano Melis
Associate III
February 21, 2024

I am monitoring the page content using the Memory renderer of STM32Cube Ide, there are values different from the erased value 0xFFFFFFFF

Adriano Melis
Associate III
February 21, 2024

AdrianoMelis_0-1708528531593.png

 

ST Employee
February 21, 2024

Hello @Adriano Melis 

The page 127 in bank1 is in 0x080F E000 - 0x080F FFFF 

the screenshot you showed, does not show page 127 

SarraS_0-1708530176754.png

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Adriano Melis
Associate III
February 21, 2024

AdrianoMelis_0-1708530610222.png

 

Adriano Melis
Associate III
February 21, 2024

my bad. this is an actual screenshot: Flash erase has been executed, FLASH content is unchanged.

(status value is HAL_OK)

 

ST Employee
February 21, 2024

Hello @Adriano Melis, 

I tried to reproduce your issue using the FLASH_EraseProgram example in STM32U5CubeFW, however, page 127 was erased successfully and I couldn't reproduce it 

Maybe share a minor project to reproduce it on my side. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Adriano Melis
Associate III
February 22, 2024

hello, these are additional info:

  • the MCU is STM32U575VGT6 on a proprietary board clocked at 100 MHz: are there known problems on this particular device? The same code is OK on the Nucleo STM32U575ZI-Q
  • FLASH erase on a single page works fine from Cube Programmer
  • when the page is pre-erased with Cube Programmer writing data is successful
ST Employee
February 22, 2024

Hello @Adriano Melis 

I suppose you're setting Flash latency to 3WS? 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Adriano Melis
Associate III
February 22, 2024

Attached two cube projects, mcb-fw-FLASH-IAP is for U575VGT (NOT working), IAP is for U575ZI (working on the Nucleo board).

As you can see the code is the same.

 

Adriano Melis
Adriano MelisAuthorBest answer
Associate III
February 23, 2024

Hello all,

I found the source of the problem: the DUALBANK bit in FLASH_OPTR was set to 1.

On this device this arranges the FLASH page access in two banks of 64 pages each.