Skip to main content
Visitor II
Apr 18, 2024 3:00 PM UTC
Question

STM32U575 Nucleo Board SMBUS

I'm new to using the Nucleo environment

 

I am not seeing any activity on the PB10 and PB11 when using the SMBUS_TwoBoards_ComIT_Master example, when looking at those pins on a scope.    I only have one board currently.

 

- Board: NUCLEO-U575ZI-Q (embeds a STM32U575ZITxQ device)

- SCL Pin: PB.10 (CN10, D36)

- SDA Pin: PB.11 (CN10, D35)

I can see CN10, but here can I see a definitive description of where D36 and D35 are on the board.

 

Also, the next stage is to read some registers in an BMS chip.  Can I use HAL_SMBUS_Master_Transmit_IT()  to read a value register value in my slave device?

This topic has been closed for replies.