Skip to main content
Łukasz Musiał
Visitor II
March 10, 2023
Question

STM32U575: is it possible to disable blocking the read and write accesses to the backup registers, backup SRAM and SRAM2 when the tamper flag is set? To use tamper input for information and not security purpose.

  • March 10, 2023
  • 1 reply
  • 696 views

According to RM: "In the NOERASE configuration (TAMPxNOER=1 in the TAMP_CR2 register, ITAMPxNOER=1 in the TAMP_CR3 register), the backup registers and other device secrets are not erased when the corresponding tamper event is detected. In addition, the read and write accesses to the backup registers and to other device secrets are blocked as soon as this potential tamper detection flag is set (tamp_potential signal, set if at least one TAMPxF or ITAMPxF is set), until this flag is cleared."

This topic has been closed for replies.

1 reply

Billy OWEN
ST Employee
March 13, 2023

Hi @?ukasz Musia?​ 

The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.

Regards,

Billy