Skip to main content
Alexmouse
Associate III
May 9, 2024
Solved

STM32U575 debug access

I've built a new prototype using the STM32U575C, and provisioned two program/debug connectors, a fine pitch Samtec header and 0,1" pitch six pin header, I've used both before on STM32F4.

I've tried accessing the processor using both headers, an STLINK-V3SET and and old F4 Nucleo.

Neither can access the processor.

Is there something fundamentally different in the U5 parts that I've missed?

I've attached the schematic of my processor sheet.

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
May 10, 2024

@Alexmouse wrote:

but I'd be happy if STLINK can just interrogate the processor.



i ask how sw you use for this. For new MCUs you require new firmware in STLink and good is not obsolete STLinkUtility, but CubeProgrammer.

18 replies

Uwe Bonnes
Chief
May 9, 2024

As you have other post her, I assumw  this is not  your first STM32 design or did you work with the debugger before. I also assume you have checked all the voltages and the board for bad solder joints. Can you perhaps check with a scope, if MCU reacts on the debugger attach tries? Does your debugger eventually allow to spy on a very low level? Any reaction at all. If there is reaction, check signal integrity. If ther is no reaction, check your board again.

Alexmouse
AlexmouseAuthor
Associate III
May 9, 2024

I've mostly used STM32F4 in the past, with various debug headers and either an STLINK pod or the debugger off a Nucleo board. This is a new design following the same principles, just with a U5 part. Voltages are correct, I will double check my pin connections to see if I've done something silly. Always a nervous moment, the first connection to the processor on a new board design.

MM..1
Super User
May 9, 2024

Start with 6pin header pins 2,3,4 only ... Check if VBAT not require power.

Alexmouse
AlexmouseAuthor
Associate III
May 9, 2024

Okay, connecting Vbat to Vdd doesn't change the symptoms.

SWCLK, SWDIO and NRST buzz through from the 6 pin header to the chip pins, which match the CubeMX pin assignments.

David Littell
Senior II
May 9, 2024

Is the core even running?  Have you tried to get the boot loader's attention at one of its ports?

How closely did you follow a known-working design like the U5 Nucleo?  What's your VDD?

Alexmouse
AlexmouseAuthor
Associate III
May 10, 2024

I've designed with reference to the datasheet and past STM32 experience, today I'll examine the Nucleo board schematics and look for potential errors. I've a Nucleo on order for further experimentation.

I'm relying upon the internal clocks as I'm pin limited and don't need precision clocks, I'm assuming the processor will default to using these?

I'm assuming basic debugger visibility in STLINK is the basic minimum interaction, how to tell what is happening inside the chip otherwise?

Vdd is 3.3 volts with SMPS generating Vcore.

Alexmouse
AlexmouseAuthor
Associate III
May 10, 2024

I've just checked Vcore, as I'm configured for SMPS, and there is 900mV present. 

Alexmouse
AlexmouseAuthor
Associate III
May 10, 2024

STLINK says:

12:10:17 : ST-LINK SN : 066CFF575450707267104359
12:10:17 : V2J43M28
12:10:17 : Connected via SWD.
12:10:17 : SWD Frequency = 100 KHz.
12:10:17 : Connection mode : Connect Under Reset.
12:10:18 : Can not connect to the target!
If you're trying to connect to an STM32W1xx device, please select Normal or HotPlug mode from Target->Settings menu.
12:10:19 : Unexpected error

MM..1
Super User
May 10, 2024

Check reset state and how sw you use?

Alexmouse
AlexmouseAuthor
Associate III
May 10, 2024

I need to scope the SWD lines, I've buzzed them thuogh to verify correct connectivity.

I was hoping to start with Blinky using CubeIDE, but I'd be happy if STLINK can just interrogate the processor.

Alexmouse
AlexmouseAuthor
Associate III
May 10, 2024

I've scoped the NRST, SWCLK & SWDIO lines on the six pin header whilst the STLINK-V3 talks to the Samtec header. I know these pins are connected to the chip. I'm not sure what I should be seeing, but at least these lines are active.