Skip to main content
Associate II
Aug 20, 2025 1:52 AM UTC
Question

STM32U535 using GPDMA and TIM2 to output a WAV file to the DAC

I have been struggling with this chip for a few days now.  I have code up for the STM32F072, and the STM32F100 series chips, but the GPDMA in the STM32U535 is baffling me.  And no, I am not a big fan of the product notes for the GPDMA, while I've gone through them, I couldn't find much to help.

Here's the challenge; the chip fails immediately with a DMA_FLAG_DTE error, with the trigger overrun flag being set in the CSR.  No idea why or where to go next after 2 days of trying to troubleshoot this.  Here is the MXCube configuration:

clock config.jpgTIM2 config.jpgDAC config1.jpggpdma config.jpg

In the code, there is a simple 8Khz WAV file stored in the "tinkles" array.  Using the standard generated code from MXCube, I have attempted to just play it out the DAC with the following calls:

HAL_DAC_Start_DMA(&hdac1, DAC_CHANNEL_1, (uint32_t*)tinkles_wav, tinkles_wav_len, DAC_ALIGN_8B_R);
HAL_TIM_Base_Start(&htim2); 

It *is* an 8-bit array, and I am not sure if that may be part of this.  Here is the code:

extern unsigned int shot_wav_len, tinkles_wav_len;
extern unsigned char shot_wav[], tinkles_wav[];
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
void HALDelayDontWork(uint32_t t) {
uint32_t s;
for (s = 0; s < t * 32222; s++) {
}
}

void HAL_DAC_ErrorCallbackCh1(DAC_HandleTypeDef *hdac) {
// while (1) {
GPIOB->ODR ^= 0x0100; //ground the bit - to turn the LED on
HALDelayDontWork(100);
GPIOB->ODR |= 0x0100; //Turn off the PCB LED
HALDelayDontWork(100);
// }
}
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_GPDMA1_Init();
 MX_DAC1_Init();
 MX_FLASH_Init();
 MX_RTC_Init();
 MX_TIM1_Init();
 MX_TIM2_Init();
 MX_USB_DRD_FS_PCD_Init();
 MX_FileX_Init();
 MX_ICACHE_Init();
 MX_SPI1_Init();
 /* USER CODE BEGIN 2 */
GPIOB->ODR |= 0x0100; //Turn off the PCB LED
GPIOB->ODR |= 0x0200; //Turn off the USB LED

HAL_DAC_Start_DMA(&hdac1, DAC_CHANNEL_1, (uint32_t*)tinkles_wav, tinkles_wav_len, DAC_ALIGN_8B_R);
HAL_TIM_Base_Start(&htim2); 

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
while (1) {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
}
 /* USER CODE END 3 */
}
And of course it is in the HAL_DAC_ErrorCallbackCh1 that we immediately wind up after a single interrupt to the GPDMA1_Channel0_IRQHandler, and a subsequent interrupt to DAC1_IRQHandler.  
 
What am I missing?
 
-D
 
 
Edited by ST Moderator to apply source code formatting. Please see the tips on how to properly insert code: How to write your question to maximize your chances to find a solution.
This topic has been closed for replies.

2 replies

Associate II
Aug 27, 2025 12:35 PM UTC

Figured it out.  The DMA_FLAG_DTE error is thrown when the source and destination address in the DAC_Start_DMA call is not expressed as a 32-bit pointer.

mƎALLEm
ST Technical Moderator
Aug 27, 2025 1:35 PM UTC

Hello,

If you solved your issue please accept your answer as solution.

Thank you.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.