Skip to main content
Associate II
February 20, 2024
Solved

STM32U535 random hard fault when running at 160 MHz

Hello.

On a custom board with STM32U535CEU6TR, I can't have HCLK set to 160 MHz. At that speed, I get random hard faults. If I set HCLK to 80 MHz, then everything is fine, no more random hard faults.

Capture d’écran de 2024-02-20 08-01-21.png

On the same board, with STM32U535CEU6QTR; no problem with HCLK set to 160 MHz.

Capture d’écran de 2024-02-20 08-01-25.png

Here is the MCU power supply (same for both boards revision) :

Capture d’écran de 2024-02-20 08-03-44.png

Clock initialization is borrowed from CubeMX generated code :

 

/* Init HAL */
HAL_Init();

/* Configure the internal regulator output voltage */
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);

/* Initialize main PLL */
RCC_OscInitTypeDef RCC_OscInitStruct = { 0, };
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
RCC_OscInitStruct.PLL.PLLM = 4;
RCC_OscInitStruct.PLL.PLLN = 40;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 1;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_0;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
HAL_RCC_OscConfig(&RCC_OscInitStruct);

/* Connect HCLK SYSCLK PCLK1 PCLK2 and PCLK3 to PLL output */
RCC_ClkInitTypeDef RCC_ClkInitStruct = { 0, };
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK |
RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_PCLK3;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4);

With STM32U535CEU6TR, if I change this line ...

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

... to this line ...

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV2;

... then I don't get random hard faults, but I don't have the expected clock frequencies I need.

For what I know, difference between Q and non-Q versions of this MCU is the non-Q version has no embedded SMPS voltage regulator. I'm not changing it, not calling HAL_PWREx_ConfigSupply(), so I assume it is set to the default reset value "LDO" (PWR_CR3 bit REGSEL).

I monitored with an oscilloscope the MCU 3V3 power supply and can't identify any issue with it.

Any help would be greatly appreciated.

 

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
February 20, 2024

Check VCAP parts actually placed.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
February 20, 2024

Check VCAP parts actually placed.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
gbm
Super User
February 20, 2024

Check if BOOSTEN bit is set in PWR->VOSR.

I have just realized that I run my U545 at 240 MHz by mistake, without any problems.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Associate II
February 20, 2024

Hi, and thanks for your reply.

VCAP capacitor is close to MCU :

Capture d’écran de 2024-02-20 08-54-19.png

On the actual board, it is present :

STM32U5.png

Thanks to your hint, I discovered that this capacitor is 10 µF while datasheet says 4.7 µF.

Changed to 4.7 µF and voilà ! MCU is now running fine at 160 MHz ! \o/

Thanks a lot !

gbm
Super User
February 20, 2024

I would rather suspect a cold joint corrected as a side effect of your fixes. Usually, but not always, bigger capacitance is better in these places.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice