Skip to main content
Associate
July 10, 2025
Solved

STM32U535 - 14 Bit ADC1 performance - getting 5bits. 12 bit ADC4 performs as expected.

I am developing a board using an STM32U535RETQ - 64 pin QFP pkg. The part is an SMPSU capable "Q" variant - although we are only using the STM's internal LDO... NOT the SMPSU.

I am using CubeMx 6.14 and StmIDE 1.18 to produce my ioc and compilation.

The 14bit ADC1 is performing as expected when set to convert internal signals - Vdd and Vbatt.

The signal to be converted is a low frequency DC signal - we're measuring current via a precision sense resistor and instrumentation amplifier.

Calibration performed during programme "init" :-

 
 
ADC_ChannelConfTypeDef sConfig = {0};

hadc1.Instance = ADC1;

sConfig.Channel = ADC_CHANNEL_3; // Ch3 intended- ******************************************

sConfig.Rank = ADC_REGULAR_RANK_1;

sConfig.SamplingTime = ADC_SAMPLETIME_12CYCLES;

sConfig.SingleDiff = ADC_SINGLE_ENDED;

sConfig.OffsetNumber = ADC_OFFSET_NONE;

sConfig.Offset = 0;



if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

{

Error_Handler();

}

if ( HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED ) != HAL_OK ) // Calibrate 14 bit ADC1 - needed to look at HAL_ADCEX driver source to determine extra ADC_Calib parameter.

{

Error_Handler(); // Handle configuration error

}

We are using the ADC in a basic mode - just one single channel to convert, started by regular software conversions.

Function to read ADC1_Ch3 :-

float Read_ADC1_Ch3(void)

{

float adc1Val;

HAL_ADC_Start(&hadc1);

HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);

adc1Val = HAL_ADC_GetValue(&hadc1); // 14 bit converter

return adc1Val;

}

When I convert any of the external channels still available ( Ch3 - the one we want, or Ch8 & Ch16 - spare I/P's ), I'm getting a cyclical swing in the reading with a 3% variation - i.e. about 5 bit performance - this repeats every several seconds.

I've looked at the I/P capacitor - nominally 1nF, values from 0-100nF have been tried without any significant difference.

Looked at the number of sample clocks - 3-814, very little difference.

The board has one, solid, Gnd plane.

ADC clock is 4MHz noimal - I've tried 250KHz-16MHz. Again - without any significant difference.

The signal I'm monitoring, measured on a 6 1/2 digit DMM is stable. The SAME SIGNAL, converted by the 12 bit ADC4 is performing as expected for a 12 bit converter. That to me almost certainly says that the issue is with the STM32 / ADC1, and not my external circuitry.

The board can be DC or battery powered - no difference on ADC1 performance.

Has anyone else encountered this issue or have any suggestions as to what the cause may be?
Thanks for any comments received.
John Haughton.

This topic has been closed for replies.
TDK
TDKBest answer
July 11, 2025

> The 14bit ADC1 is performing as expected when set to convert internal signals - Vdd and Vbatt.

This indicates ADC1 is working okay. It's the same circuitry after the sampling cap for all channels.

Recheck your assumptions. Missing something.

Show a plot of the bad data if you can. Might provide some clues. What frequency is the noise? FFT may also prove insightful.

"If you feel a post has answered your question, please click ""Accept as Solution""."

7 replies

TDK
TDKBest answer
July 11, 2025

> The 14bit ADC1 is performing as expected when set to convert internal signals - Vdd and Vbatt.

This indicates ADC1 is working okay. It's the same circuitry after the sampling cap for all channels.

Recheck your assumptions. Missing something.

Show a plot of the bad data if you can. Might provide some clues. What frequency is the noise? FFT may also prove insightful.

"If you feel a post has answered your question, please click ""Accept as Solution""."
JLH64Author
Associate
July 11, 2025

I've checked whether an ADC4 chanel, using the same physical pin as an ADC1 chanel, is performing within expectations - it is.

I've also cut down the code so that the only peripherals initialised are ADC1, GPIO, and the ICACHE :-

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
// MX_RTC_Init();
 // MX_TIM2_Init();
// MX_LPTIM1_Init();
 MX_ICACHE_Init();
// MX_DAC1_Init();
 MX_ADC1_Init();
 /* USER CODE BEGIN 2 */

All that is left in the main loop is :-

 while (1)
 {
	 adcVal = Read_ADC1_Ch3();
	 HAL_Delay(5);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */

Setting a breakpoint on the HAL_Delay, and inspecting "adcVal"confirms that internal signals are performing to expectations, whilst external signals are unusable.

In operation, the device only needs to read the i/p signal several times a second. To get a picture of the noise I'll create an array and see if I can get it into XL, or spit the values out of DAC1 ( which is performing to expectations).

GaetanGodart
ST Employee
July 14, 2025

Hello @JLH64 ,

 

The cyclical variation is related to the input multiplexer switching during the ADC's successive approximation process.
ADC4 works fine because it has its own independent input multiplexer and sampling mechanism, so it does not suffer from the same issue as ADC1.

A solution could be to use continuous conversion mode for the same channel, this keeps the input multiplexer fixed on the selected channel, avoiding disturbances from switching.
You could also try to increase the sampling time, allowing more time for the ADC to stabilize can help reduce noise. Ensure the ADC clock and sampling time are within the recommended ranges.
Finally, you could duplicate each channel in the scan sequence, in scan mode, set the sequence so that each channel is converted twice in a row. Discard the first result and use the second, as the first may be affected by switching noise.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
mƎALLEm
ST Technical Moderator
July 11, 2025

Hello @JLH64 ,

I've edited your post to follow the ST community rules. So in next time please use </> button to share your code. Please review this post.

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
JLH64Author
Associate
July 11, 2025

Update - I have confirmed that the issue is still present on other boards, two variants - my developement set, with signal conditioning, as well as prototype production boards, where I currently only have a direct input to ADC1_Ch3 (the signal conditioning will be on an I/O board.

Using a reference voltage, direct into the ADC, gives me the same results as above.
I have also cut the project down so that the only peripherals initialised are ADC1 and the GPIO.

All other hardware ( pretty minimal - LCD driver, external comparator ) is powered down.