STM32U5 Max LSE bypass frequency documentation error
In STM32U575/585 RM0456 Rev 2 from September 2021, I see the following:
"11.4.7 LSE clock
...
External source (LSE bypass)
In this mode, an external clock source must be provided. It can have a frequency of up to 1 MHz."
However, in STM32U585xx DS13086 Rev 4 from December 2021, I see the following:
"5.3.7 External clock timing characteristics
...
Table 78. Low-speed external user clock characteristics
f_LSE_ext - User external clock source frequency
Min: 5 kHz
Typ: 32.768 kHz
Max: 40 kHz"
So, is the max LSE frequency in bypass mode 1 MHz or is it 40 kHz? On previous MCU families such as the STM32G4 an LSE frequency up to 1 MHz in bypass mode was supported.
Thanks!