Skip to main content
Matteo Cardani
Associate II
October 26, 2022
Solved

STM32U5 ADC calibration

Hello,

I'm using an ST32U5 microcontroller and I'd like to ask some question about the ADC linear and offset calibration feature.

1 - This feature is only available on ADC1 or is it also available on ADC4?

2 - Right now at startup I'm launching the ADC1 calibration with the following parameter :ADC_CALIB_OFFSET_LINEARITY. Does this calibrate both the offset and the gain?

3 - Is there some issues (except for a longer startup time) in launching the calibration every time at startup?

Thank you

Matteo

This topic has been closed for replies.
_andreas
_andreasBest answer
Senior
October 26, 2022

The ADC4 has only offset calibration, see page 1084 in RM0456 Rev 3

The ADC1 can do both, and ADC_CALIB_OFFSET_LINEARITY

should calibrate offset and linearity.

2 replies

_andreas
_andreasBest answer
Senior
October 26, 2022

The ADC4 has only offset calibration, see page 1084 in RM0456 Rev 3

The ADC1 can do both, and ADC_CALIB_OFFSET_LINEARITY

should calibrate offset and linearity.

Matteo Cardani
Associate II
November 2, 2022

Thank you!