Skip to main content
Associate III
August 7, 2024
Question

STM32U5: 2 NMI generated upon 2-bit Flash ECC error.

Hi ,

I am working on to implement functionality to detect flash 2 bit ECC error. To test my implementation followed below method in STM32U5 reference manual. With this method,  I am able to generate flash 2 bit ECC error.

harisuvarna_0-1723045561610.png

However I have following observations

  •  SYS_ECC  bit in FLASH_ECCR register sets upon NMI generation and never clears
  •  2 NMI interrupts generated instead of 1. 

Is this is expected behavior. Please clarify.

Regards,

Hareesha

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
August 7, 2024

>>2 NMI interrupts generated

You leave the NMI Handler? Without clearing the source?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate III
August 7, 2024

Hi,

Thanks for the quick response. In my case source of the NMI is 2-bit Flash ECC error. Hence I cleared corresponding 

flag (ECCD) by writing to 1 bit ECCD in register FLASH_ECCR.

Regards,

Hareesha