Skip to main content
Associate II
Jul 10, 2026 3:43 PM UTC
Solved

STM32U3C5: HSP Interrupts

I am trying to generate an interrupt when the HSP finishes a processing list so that I don’t need to poll it. However, I can’t seem to figure out how to do this.

There are some things in the STM32U3 reference manual that make me confused:

In section 19.4.12 HSP interrupt controller (HITC), there are four interrupt lines:
• An interrupt line handling errors (hsp_err_it)

• An interrupt line handling various hardware events (hsp_evt_it)

• An interrupt line handling events generated by the SPE processing (hsp_fwevt_it)

• A global interrupt is asserted when one of the previous interrupts is asserted (hsp_it)

However, in Section 19.3 HSP Implementation, Table 143 shows that neither hsp_err_it, hsp_evt_it, nor hsp_fwevt_it are implemented in the U3 series. If this is the case, does that mean that hsp_it is just never asserted? Is it possible to notify the application when a processing list has finished without polling for a flag?

Section 5.13.5 of UM3360: HSP processing functions says that the SET_FLAG function can generate an interrupt when it sets a bit in HSP_PFCTEVT_ISR, but is this mapped to one of the unimplemented lines?

I am using STM32U3C5

PVXBest answer
ST Employee
Aug 14, 2026 6:08 PM UTC

Hi @AQB,

You can indeed use the SET_FLAG command to signal the end of an HSP processing list (or any other relevant user event) by interrupting the CPU on STM32U3C5/B5, as you originally planned to do.

Polling is usually not necessary with the HSP because it is designed for efficient interrupt-driven synchronization with the CPU and other HW elements.

The ‘unconnected’ lines hsp_err_it, hsp_fwevt_it, hsp_evt_it lines are actually wired-or together to create the global interrupt line hsp_it, as shown in diagram 19.4.12 in the reference manual, so any condition that triggers one of the Iines (an error, a hardware event or a FW processing event) will also trigger the HSP global interrupt line.

To achieve the desired effect, you will need to enable the HSP_PFCTEVT_IER register bit corresponding to the processing event number you are going to trigger in your application, in the range 0-31.

Please note that, since the global interrupt may be triggered by other conditions (e.g. HSP errors), it is advisable to check the HSP_ERR_ISR and HSP_EVT_ISR registers for possible HW events before checking the HSP_PFCTEVT_ISR register for FW processing events inside the CPU-side ISR.

Best regards and good work on your application 🙂

 

*Edited to correct a typo in the interrupt enable register name (previous: HSP_PFCTEVT_ISR, corrected: HSP_PFCTEVT_IER) 

3 replies

AQBAuthor
Associate II
Jul 10, 2026 6:47 PM UTC

My workaround for now is to use a SetTrgo function at the end of the processing list, and this Trgo triggers a DMA channel to move a single dummy byte. I can then use the DMA’s callback as the HSP complete callback.

ST Technical Moderator
Jul 15, 2026 11:21 AM UTC

Hi ​@AQB 

Only global interrupt is implemented in STM32U3C5/B5. hsp_err_it hsp_fwevt_it hsp_evt_it are not connected. So to notify about a HW event or processing list completion, you need to poll for a flag as implemented in HAL.

It is not possible to use the SET_FLAG command to interrupt the CPU on STM32U3C5/B5, and a polling mechanism is required.

UPDATE : After checking with our expert ​@PVX it should be possible to interrupt the cpu by set_flag() even if the specific interrupt hsp_fwevt_it is not implemented
An internal ticket is submitted to dedicated team CDM0065255

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
PVXBest answer
ST Employee
Aug 14, 2026 6:08 PM UTC

Hi @AQB,

You can indeed use the SET_FLAG command to signal the end of an HSP processing list (or any other relevant user event) by interrupting the CPU on STM32U3C5/B5, as you originally planned to do.

Polling is usually not necessary with the HSP because it is designed for efficient interrupt-driven synchronization with the CPU and other HW elements.

The ‘unconnected’ lines hsp_err_it, hsp_fwevt_it, hsp_evt_it lines are actually wired-or together to create the global interrupt line hsp_it, as shown in diagram 19.4.12 in the reference manual, so any condition that triggers one of the Iines (an error, a hardware event or a FW processing event) will also trigger the HSP global interrupt line.

To achieve the desired effect, you will need to enable the HSP_PFCTEVT_IER register bit corresponding to the processing event number you are going to trigger in your application, in the range 0-31.

Please note that, since the global interrupt may be triggered by other conditions (e.g. HSP errors), it is advisable to check the HSP_ERR_ISR and HSP_EVT_ISR registers for possible HW events before checking the HSP_PFCTEVT_ISR register for FW processing events inside the CPU-side ISR.

Best regards and good work on your application 🙂

 

*Edited to correct a typo in the interrupt enable register name (previous: HSP_PFCTEVT_ISR, corrected: HSP_PFCTEVT_IER)