STM32U375 STOP3 mode: IWDG resets the device although IWDG_STOP option byte is set to Freeze
Hello,
I am using an STM32U375 and trying to enter STOP3 mode without any wakeup source.
Device configuration
Option Bytes:
IWDG_SW = 1
IWDG_STOP = 0
IWDG_STDBY = 1
According to RM, IWDG_STOP = 0 means:
Bit 17 IWDG_STOP:
0: IWDG counter frozen in Stop mode
1: IWDG counter running in Stop mode
The OPTR register value is:
FLASH->OPTR = 0x1FEDF0AA
IWDG configuration
C
hiwdg.Instance = IWDG;
hiwdg.Init.Prescaler = IWDG_PRESCALER_256;
hiwdg.Init.Window = 4095;
hiwdg.Init.Reload = 4095;
hiwdg.Init.EWI = 0;
HAL_IWDG_Init(&hiwdg);
Expected timeout is approximately 32.8 seconds (LSI ≈ 32 kHz).
STOP3 entry sequence
Before entering STOP3 I clear all wakeup-related flags:
C
RTC->SCR = 0xFFFFFFFF;
TAMP->SCR = 0xFFFFFFFF;
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_STOPF);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SBF);
PWR->WUSCR = 0xFFFFFFFF;
EXTI->RPR1 = 0xFFFFFFFF;
EXTI->FPR1 = 0xFFFFFFFF;
SysTick->CTRL = 0;
SCB->ICSR = SCB_ICSR_PENDSTCLR_Msk;
Then:
C
MODIFY_REG(PWR->CR1,
PWR_CR1_LPMS,
PWR_CR1_LPMS_0 | PWR_CR1_LPMS_1); // STOP3
SET_BIT(SCB->SCR, SCB_SCR_SLEEPDEEP_Msk);
HAL_IWDG_Refresh(&hiwdg);
__DSB();
__ISB();
__WFI();
What I observed
Before executing __WFI():
PWR->CR1 LPMS = STOP3
SCB->SCR SLEEPDEEP = 1
Wakeup-related flags:
PWR WUFx = 0
NVIC->ISPR[0] = 0
NVIC->ISPR[1] = 0
RTC state:
RTC->ICSR = 0x27
WUTWF = 1
UART status only shows normal flags:
TC = 1
TXFNF = 1
After entering STOP3, code execution never reaches the statement following __WFI().
However, after approximately 30-33 seconds, the device resets and:
RCC reset flags:
IWDGRSTF = 1
The reset interval matches the configured IWDG timeout.
My question
Based on the documentation, I would expect the IWDG to be frozen in STOP mode because:
IWDG_STOP = 0
However, the observed behavior suggests that the IWDG continues running while the device is in STOP3.
Is there any known limitation, errata, or specific condition on STM32U375 where:
- IWDG continues running in STOP3 despite
IWDG_STOP = 0, or - STOP3 behaves differently from other STOP modes regarding IWDG freeze?
Any guidance would be appreciated.
Thanks.